Other Parts Discussed in Thread: LM25017
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM25017您好!
我们正在寻找具有多个输出的单个 IC、其要求如下:
输入:28V
输出1:5V 和300mA
输出2:(-12V)和50mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.