Other Parts Discussed in Thread: LM5157-Q1
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5177 主题中讨论的其他器件:LM5157-Q1
工具与软件:
我需要一个能够接受6V 至48V 输入范围并提供15V/1A 输出的 IC。 此外、IC 应包含功能安全特性并具有内部 MOSFET。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.