主题中讨论的其他器件:UNIFLASH、
尊敬的 TI 社区:
我已经阅读了很多有关将 TI UniFlash 工具与非 FTDI USB 转 UART 桥结合使用的 E2E 主题。
尽管据说 CP2102应该兼容、但我没有成功地对 CC3200器件进行编程、并且无论我使用的是 GUI 中的哪个命令、都会不断地收到相同的错误:
[10:55:45] Begin Program operation. [10:55:45] INFO: > Executing Operation: Connect [10:55:48] INFO: setting break signal [10:55:49] INFO: detecting FTDI for device reset [10:55:49] ERROR: No device USB ports were found [10:55:49] INFO: --- please restart the device --- [10:56:03] ERROR: ---reading ACK signal failed--- [10:56:03] WARNING: ---seting break signal to false failed--- [10:56:05] INFO: setting break signal [10:56:06] INFO: detecting FTDI for device reset [10:56:06] ERROR: No device USB ports were found [10:56:06] INFO: --- please restart the device --- [10:56:23] ERROR: ---reading ACK signal failed--- [10:56:23] WARNING: ---seting break signal to false failed--- [10:56:25] INFO: setting break signal [10:56:27] INFO: detecting FTDI for device reset [10:56:27] ERROR: No device USB ports were found [10:56:27] INFO: --- please restart the device ---
我的 UniFlash 版本应该为1到2年(提供了屏幕截图)。
那么、我的问题如下: UniFlash 的当前状态是什么、它是否可用于 CP2102 (或任何其他非 FTDI 桥接器)?
提前感谢您!