主题中讨论的其他器件:CC3220SF、 UNIFLASH
您好!
目前、我将使用自定义 CC3220SF 以及 TI_Azure SDK (azure_cc32xx_4_10_01_01)。
TI -主机驱动程序版本(主机驱动程序版本:3.0.1.61)和 sp_3.15.0.1_2.0.0.0_2.2.0.7.bin -刷新的服务包版本。
刷写二进制文件(首次刷写二进制文件)后、我将尝试使用第三方 HTTP-Client (安装在移动设备中)来执行 HTTP-GET / HTTP POST。 器件未响应(未向主机处理器提供任何事件)。
只有在刷写二进制文件后才会观察到这种行为。 重置 MCU 后、HTTP-GET / POST 将按预期工作。
请查找随附的日志以供参考(故障情况)-刷写二进制文件(首次)后
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Debug] Post connectionAsyncEvent [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Debug] Post connectionAsyncEvent [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Debug] Post connectionAsyncEvent Device came up in Access-Point mode Switching Networking mode on application request Device came up in Station mode RestAPI_Notify(): ProvisioningStarted [Provisioning task] Provisioninig task initialized [Provisioning task] watchdog registration done with handle=1 [Provisioning task] Wake up on Power ON [Provisioning task] Device started as STATION [Provisioning task] validateLocalLinkConnection() sem wait [WLAN EVENT] Auto-Provisioning Started [Provisioning task] validateLocalLinkConnection() sem exit ret=0, status=0 [Provisioning task] Cannot connect to AP or profile does not exist RestAPI_Notify(): ProvisioningStopped [WLAN EVENT] Provisioning stopped [WLAN EVENT] - WLAN Connection Status:0 [Provisioning task] detected device is CC3220SF [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Debug] Post connectionAsyncEvent [Provisioning task] Device is configured in default state [Provisioning task] Current: 0, Event: 0, Next: 1 [Provisioning task] Device started in AP role [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Debug] Post connectionAsyncEvent [Provisioning task] Host Driver Version: 3.0.1.61 [Provisioning task] Build Version 3.15.0.1.31.2.0.0.0.2.2.0.7 [Provisioning task] Starting Provisioning - [Provisioning task] in mode 2 (0 = AP, 1 = SC, 2 = AP+SC) [Provisioning task] Provisioning Started. Waiting to be provisioned..!! [Provisioning task] Current: 1, Event: 1, Next: 2 ========================>>>>>>>>>>>>>>>>>>>>>> Here trying for HTTP-GET & HTTP - POST
重置(硬件重置)后、请查找日志(成功案例)。
[Debug] Post connectionAsyncEvent [Provisioning task] Host Driver Version: 3.0.1.61 [Provisioning task] Build Version 3.15.0.1.31.2.0.0.0.2.2.0.7 [Provisioning task] Starting Provisioning - [Provisioning task] in mode 2 (0 = AP, 1 = SC, 2 = AP+SC) [Provisioning task] Provisioning Started. Waiting to be provisioned..!! [Provisioning task] Current: 1, Event: 1, Next: 2 CertGET(): certificate sent ====>>>>>> HTTP-GET success case ConfigGET() = Configuration sent
此致、
Suresh