This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3220SF-LAUNCHXL:TI_Azure SDK -通过 UNIFLASH 刷写映像后、HTTP GET 和 HTTP POST 不起作用(仅限第一个)

Guru**** 2540720 points
Other Parts Discussed in Thread: CC3220SF, UNIFLASH

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1033428/cc3220sf-launchxl-ti_azure-sdk---http-get-and-http-post-not-working-after-flashing-the-image-through-uniflash-only-first

器件型号:CC3220SF-LAUNCHXL
主题中讨论的其他器件:CC3220SFUNIFLASH

您好!

目前、我将使用自定义 CC3220SF 以及 TI_Azure SDK (azure_cc32xx_4_10_01_01)。


TI -主机驱动程序版本(主机驱动程序版本:3.0.1.61) sp_3.15.0.1_2.0.0.0_2.2.0.7.bin -刷新的服务包版本。

  

刷写二进制文件(首次刷写二进制文件)后、我将尝试使用第三方 HTTP-Client (安装在移动设备中)来执行 HTTP-GET / HTTP POST。 器件未响应(未向主机处理器提供任何事件)。

只有在刷写二进制文件后才会观察到这种行为。 重置 MCU 后、HTTP-GET / POST 将按预期工作。

  

请查找随附的日志以供参考(故障情况)-刷写二进制文件(首次)后

[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1

[Debug] Post connectionAsyncEvent
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1

[Debug] Post connectionAsyncEvent
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1

[Debug] Post connectionAsyncEvent
Device came up in Access-Point mode

Switching Networking mode on application request

Device came up in Station mode

RestAPI_Notify(): ProvisioningStarted

[Provisioning task] Provisioninig task initialized

[Provisioning task] watchdog registration done with handle=1
[Provisioning task] Wake up on Power ON

[Provisioning task] Device started as STATION

[Provisioning task] validateLocalLinkConnection() sem wait

[WLAN EVENT] Auto-Provisioning Started

[Provisioning task] validateLocalLinkConnection() sem exit ret=0, status=0

[Provisioning task] Cannot connect to AP or profile does not exist

RestAPI_Notify(): ProvisioningStopped

[WLAN EVENT] Provisioning stopped

 [WLAN EVENT] - WLAN Connection Status:0

[Provisioning task] detected device is CC3220SF

[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1

[Debug] Post connectionAsyncEvent
[Provisioning task] Device is configured in default state

[Provisioning task] Current: 0, Event: 0, Next: 1

[Provisioning task] Device started in AP role

[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1

[Debug] Post connectionAsyncEvent
[Provisioning task] Host Driver Version: 3.0.1.61

[Provisioning task] Build Version 3.15.0.1.31.2.0.0.0.2.2.0.7

[Provisioning task] Starting Provisioning -
[Provisioning task] in mode 2 (0 = AP, 1 = SC, 2 = AP+SC)

[Provisioning task] Provisioning Started. Waiting to be provisioned..!!

[Provisioning task] Current: 1, Event: 1, Next: 2

========================>>>>>>>>>>>>>>>>>>>>>> Here trying for HTTP-GET & HTTP - POST

重置(硬件重置)后、请查找日志(成功案例)。

[Debug] Post connectionAsyncEvent
[Provisioning task] Host Driver Version: 3.0.1.61

[Provisioning task] Build Version 3.15.0.1.31.2.0.0.0.2.2.0.7

[Provisioning task] Starting Provisioning -
[Provisioning task] in mode 2 (0 = AP, 1 = SC, 2 = AP+SC)

[Provisioning task] Provisioning Started. Waiting to be provisioned..!!

[Provisioning task] Current: 1, Event: 1, Next: 2


CertGET(): certificate sent   ====>>>>>> HTTP-GET success case
ConfigGET() = Configuration sent


此致、
Suresh  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Suresh、

    您的应用程序似乎正在启动和停止配置。 您是否连接到接入点?

    此致、

    Sarah

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Sarah、  

    非常感谢您的回答。  

     

    移动应用能够连接到器件的 AP、还可以使用"/api/1/wlan/profile_add  "HTTP API 添加 WLAN 配置文件。

    只有自定义 HTTP-Get/ POST 出现问题才会发送到应用程序。

    (如果没有特定于应用的自定义 HTTP GET / POST、则可以配置器件)。

    此致、

    Suresh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Sarah、  

    我 认为 UniFlash 默认设置造成了这个问题。 变化   

    角色设置>常规设置> 自动配置以禁用已解决的我的问题

    此致、

    Suresh