Other Parts Discussed in Thread: CC3100
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC3100 工具/软件:Code Composer Studio
你(们)好
我已经看到 CC3100在 AP 模式下使用大约66mA (5V 时)。
是否可以降低此功耗? 设置 sl_low_power_policy 或降低 TX 功率不起作用。
谢谢
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.