请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:WL1807MOD 您好!
WL1807MOD 模块支持2.4GHz 和5GHz。
默认情况下是否启用5GHz 功能? 我们的应用仅需要2.4GHz (工业)。
如果默认启用了5GHz (STA/AP)功能、如何禁用该功能?
请告诉我禁用5GHz 的设置。
此致
库米
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.