请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC2538 主题: CC2592中讨论的其他部件
我使用的是由cc2538和cc2592组成的自定义设计。 除了无线电性能之外,设计似乎还可以,但在检查cc2538的参考原理图和阅读数据表时,我感到困惑的是:
针4 (CC2538的),即DVDD_USB,如果DVDD,AVDD和AVDD_GUARD线路全部与3.3V电源短路,则可绑带至3.3V或无。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的是由cc2538和cc2592组成的自定义设计。 除了无线电性能之外,设计似乎还可以,但在检查cc2538的参考原理图和阅读数据表时,我感到困惑的是:
针4 (CC2538的),即DVDD_USB,如果DVDD,AVDD和AVDD_GUARD线路全部与3.3V电源短路,则可绑带至3.3V或无。
谢谢。