请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC2530 尊敬的所有人:
在使用CC2530测量个体的过程中,我们发现传输功率偏差非常大, 传输功率为2-5.5dBm, 交叉测试,5DB模块的输出功率和2dB模块的输出功率可与CC2530芯片互换,发现该板不影响,由输出功率差异引起的芯片。
问题是:CC2530芯片数据表描述了典型输出功率为4.5dB,为什么会出现这样的结果?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.