This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-CC2652R7:构建错误

Guru**** 2943350 points

Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1178047/lp-cc2652r7-build-errors

器件型号:LP-CC2652R7
主题中讨论的其他器件:CC2652R7SYSBIOSSIMPLELINK-CC13XX-CC26XX-SDK

你(们)好

我正在尝试从 simplelink SDK 构建 pwmled2示例。

我已经尝试了全部3个示例- NoRTOS、FreeRTOS 和 TIRTOS。 这三个都无法构建。 每个构建日志如下所示:

NoRTOS:

**** Build of configuration Debug for project pwmled2_LP_CC2652R7_nortos_gcc ****

/home/vivek/ti/ccs1210/ccs/utils/bin/gmake -k -j 16 all -O 
 
Building target: "pwmled2_LP_CC2652R7_nortos_gcc.out"
Invoking: GNU Linker
"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/arm-none-eabi-gcc-9.2.1" -mfpu=fpv4-sp-d16 -DDeviceFamily_CC26X2X7 -O3 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -mcpu=cortex-m4 -Wl,-Map,"pwmled2_LP_CC2652R7_nortos_gcc.map" --entry resetISR -nostartfiles -static -Wl,--gc-sections -L"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -L"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/nortos" -L"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_nortos_gcc/Debug/syscfg" -L"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/lib/thumb/v7e-m/hard" -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 --specs=nano.specs -o"pwmled2_LP_CC2652R7_nortos_gcc.out" "./main_nortos.o" "./pwmled2.o" "./syscfg/ti_devices_config.o" "./syscfg/ti_drivers_config.o" -Wl,-T"../cc13x2x7_cc26x2x7_nortos.lds"  -l:ti_utils_build_linker.cmd.genlibs -l:"ti/devices/cc13x2x7_cc26x2x7/driverlib/bin/gcc/driverlib.lib" -lgcc -lc -lm -lnosys 
makefile:147: recipe for target 'pwmled2_LP_CC2652R7_nortos_gcc.out' failed
/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/../../../../arm-none-eabi/bin/ld: /home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/liblto_plugin.so: error loading plugin: /home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/liblto_plugin.so: file too short
collect2: error: ld returned 1 exit status
gmake[1]: *** [pwmled2_LP_CC2652R7_nortos_gcc.out] Error 1
gmake: *** [all] Error 2
makefile:143: recipe for target 'all' failed

FreeRTOS:

**** Build of configuration Debug for project pwmled2_LP_CC2652R7_freertos_gcc ****

/home/vivek/ti/ccs1210/ccs/utils/bin/gmake -k -j 16 all -O 
 
Building file: "syscfg/ti_freertos_portable_config.c"
Invoking: GNU Compiler
"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/arm-none-eabi-gcc-9.2.1" -c -mcpu=cortex-m4 -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -DDeviceFamily_CC26X2X7 -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/freertos" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/posix/gcc" -I"/FreeRTOS/Source/include" -I"/FreeRTOS/Source/portable/GCC/ARM_CM4F" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include/newlib-nano" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include" -O3 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF"syscfg/ti_freertos_portable_config.d_raw" -MT"syscfg/ti_freertos_portable_config.o" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug/syscfg" -std=c99  -o"syscfg/ti_freertos_portable_config.o" "syscfg/ti_freertos_portable_config.c"
subdir_rules.mk:33: recipe for target 'syscfg/ti_freertos_portable_config.o' failed
syscfg/ti_freertos_portable_config.c:14:10: fatal error: ../portable/GCC/ARM_CM4F/port.c: No such file or directory
   14 | #include <../portable/GCC/ARM_CM4F/port.c>
      |          ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
gmake: *** [syscfg/ti_freertos_portable_config.o] Error 1
../main_freertos.c:46:10: fatal error: FreeRTOS.h: No such file or directory
   46 | #include <FreeRTOS.h>
      |          ^~~~~~~~~~~~
compilation terminated.
gmake: *** [main_freertos.o] Error 1
syscfg/ti_freertos_config.c:24:10: fatal error: ../../Source/list.c: No such file or directory
   24 | #include <../../Source/list.c>
      |          ^~~~~~~~~~~~~~~~~~~~~
compilation terminated.
gmake: *** [syscfg/ti_freertos_config.o] Error 1
Building file: "../main_freertos.c"
Invoking: GNU Compiler
"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/arm-none-eabi-gcc-9.2.1" -c -mcpu=cortex-m4 -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -DDeviceFamily_CC26X2X7 -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/freertos" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/posix/gcc" -I"/FreeRTOS/Source/include" -I"/FreeRTOS/Source/portable/GCC/ARM_CM4F" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include/newlib-nano" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include" -O3 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF"main_freertos.d_raw" -MT"main_freertos.o" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug/syscfg" -std=c99  -o"main_freertos.o" "../main_freertos.c"
subdir_rules.mk:7: recipe for target 'main_freertos.o' failed
Building file: "syscfg/ti_freertos_config.c"
Invoking: GNU Compiler
"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/arm-none-eabi-gcc-9.2.1" -c -mcpu=cortex-m4 -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -DDeviceFamily_CC26X2X7 -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/freertos" -I"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/posix/gcc" -I"/FreeRTOS/Source/include" -I"/FreeRTOS/Source/portable/GCC/ARM_CM4F" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include/newlib-nano" -I"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/include" -O3 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF"syscfg/ti_freertos_config.d_raw" -MT"syscfg/ti_freertos_config.o" -I"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_freertos_gcc/Debug/syscfg" -std=c99  -o"syscfg/ti_freertos_config.o" "syscfg/ti_freertos_config.c"
subdir_rules.mk:33: recipe for target 'syscfg/ti_freertos_config.o' failed
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

TIRTOS:

**** Build of configuration Debug for project pwmled2_LP_CC2652R7_tirtos7_gcc ****

/home/vivek/ti/ccs1210/ccs/utils/bin/gmake -k -j 16 all -O 
 
Building target: "pwmled2_LP_CC2652R7_tirtos7_gcc.out"
Invoking: GNU Linker
"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/arm-none-eabi-gcc-9.2.1" -mfpu=fpv4-sp-d16 -DDeviceFamily_CC26X2X7 -O3 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -mcpu=cortex-m4 -Wl,-Map,"pwmled2_LP_CC2652R7_tirtos7_gcc.map" -nostartfiles -static -Wl,--gc-sections -L"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -L"/home/vivek/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/tirtos7/packages" -L"/home/vivek/workspace_v12/pwmled2_LP_CC2652R7_tirtos7_gcc/Debug/syscfg" -L"/home/vivek/ti/gcc_arm_none_eabi_9_2_1/arm-none-eabi/lib/thumb/v7e-m/hard" -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 --specs=nano.specs -o"pwmled2_LP_CC2652R7_tirtos7_gcc.out" "./main_tirtos.o" "./pwmled2.o" "./syscfg/ti_devices_config.o" "./syscfg/ti_drivers_config.o" "./syscfg/ti_sysbios_config.o" -Wl,-T"../cc13x2x7_cc26x2x7_tirtos7.lds"  -l:ti_utils_build_linker.cmd.genlibs -l:"ti/devices/cc13x2x7_cc26x2x7/driverlib/bin/gcc/driverlib.lib" -lgcc -lc -lm -lnosys 
makefile:148: recipe for target 'pwmled2_LP_CC2652R7_tirtos7_gcc.out' failed
/home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/../../../../arm-none-eabi/bin/ld: /home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/liblto_plugin.so: error loading plugin: /home/vivek/ti/gcc_arm_none_eabi_9_2_1/bin/../lib/gcc/arm-none-eabi/9.2.1/liblto_plugin.so: file too short
collect2: error: ld returned 1 exit status
gmake[1]: *** [pwmled2_LP_CC2652R7_tirtos7_gcc.out] Error 1
gmake: *** [all] Error 2
makefile:144: recipe for target 'all' failed

**** Build Finished ****

如何解决错误?

其他几个问题:

1) 1)在哪里可以了解 FreeRTOS 和 TIRTOS 之间的差异

2) 2)从哪里可以学习从头开始构建项目? 项目中发生的事情太多了、我想了解一下这些事情。

非常感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Vivek、

    请查看 SIMPLELINK-CC13XX-CC26XX-SDK 发行说明 、了解应使用的正确相关性。

    您需要单独安装 GCC 和 FreeRTOS、并确保 Project Properties -> Resources -> Linked Resources and  Project Properties -> CCS Build-> Environment 路径正确。  您的 GCC 目录似乎返回错误"file too short"、必须解决该错误。  例如、我的 GCC FreeRTOS 项目使用以下链接资源进行构建:

    您可以查看 SDK 用户指南 以了解 FreeRTOS 和 TI-RTOS 之间的差异、并使用 项目开始空白开发。

    此致、
    Ryan