This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2652R7:如何在连接到 openthread 网络时降低功耗?

Guru**** 2928980 points

Other Parts Discussed in Thread: CC2652R7, ENERGYTRACE, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1385285/cc2652r7-how-to-reduce-the-power-consumption-when-connecting-to-an-openthread-network

器件型号:CC2652R7
Thread 中讨论的其他器件: ENERGYTRACESysConfig

工具与软件:

SDK:SimpleLink CC13xx CC26xx SDK (6.41.00.17)

TI 温度传感器示例:temp_sensor_lp_CC2652R7_tirtos7_ticlang

经测试、连接至 openthread 网络时、第一个连接(即 openthread 网络中没有超时记录)消耗的电流为6~7mA、而其他连接消耗的电流为2~3mA。

我想问的是、是否可以降低此电流消耗?

谢谢你