This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335 ADC to DMA



从TI网站上下载的demo程序可以采集A0,A1,A2,A3四个通道,但是我想改成A0一个通道,怎么修改?附上原始程序和修改后的程序(但不能很好工作,采用得到的A0通道数据和输入信号存在非常大的差别)

原始程序

//###########################################################################  

//  

// FILE:   Example_2833xAdcToDMA.c  

//  

// TITLE:  DSP2833x ADC To DMA  

// ASSUMPTIONS:  

//  

//    This program requires the DSP2833x header files.  

//  

//    Make sure the CPU clock speed is properly defined in  

//    DSP2833x_Examples.h before compiling this example.  

//  

//    Connect the signals to be converted to channel A0, A1, A2, and A3.  

//  

//    As supplied, this project is configured for "boot to SARAM"  

//    operation.  The 2833x Boot Mode table is shown below.  

//    For information on configuring the boot mode of an eZdsp,  

//    please refer to the documentation included with the eZdsp,  

//  

//       $Boot_Table:  

//  

//         GPIO87   GPIO86     GPIO85   GPIO84  

//          XA15     XA14       XA13     XA12  

//           PU       PU         PU       PU  

//        ==========================================  

//            1        1          1        1    Jump to Flash  

//            1        1          1        0    SCI-A boot  

//            1        1          0        1    SPI-A boot  

//            1        1          0        0    I2C-A boot  

//            1        0          1        1    eCAN-A boot  

//            1        0          1        0    McBSP-A boot  

//            1        0          0        1    Jump to XINTF x16  

//            1        0          0        0    Jump to XINTF x32  

//            0        1          1        1    Jump to OTP  

//            0        1          1        0    Parallel GPIO I/O boot  

//            0        1          0        1    Parallel XINTF boot  

//            0        1          0        0    Jump to SARAM       <- "boot to SARAM"  

//            0        0          1        1    Branch to check boot mode  

//            0        0          1        0    Boot to flash, bypass ADC cal  

//            0        0          0        1    Boot to SARAM, bypass ADC cal  

//            0        0          0        0    Boot to SCI-A, bypass ADC cal  

//                                              Boot_Table_End$  

//  

//  

// DESCRIPTION:  

//  

// ADC is setup to convert 4 channels for each SOC received, with  total of 10 SOCs.  

// Each SOC initiates 4 conversions.  

// DMA is set up to capture the data on each SEQ1_INT.  DMA will re-sort      

// the data by channel sequentially, i.e. all channel0 data will be together  

// all channel1 data will be together.  

//  

// Code should stop in local_DINTCH1_ISR when complete  

//  

// Watch Variables:  

//      DMABuf1  

//  

//###########################################################################  

//  

// Original source by: M.P.  

//  

// $TI Release: DSP2833x Header Files V1.10 $  

// $Release Date: February 15, 2008 $  

//###########################################################################  

#include "DSP2833x_Device.h"     // DSP2833x Headerfile Include File  

#include "DSP2833x_Examples.h"   // DSP2833x Examples Include File  

// ADC start parameters  

#if (CPU_FRQ_150MHZ)     // Default - 150 MHz SYSCLKOUT  

 #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3)   = 25.0 MHz  

#endif  

#if (CPU_FRQ_100MHZ)  

 #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2)   = 25.0 MHz  

#endif  

#define ADC_CKPS   0x1   // ADC module clock = HSPCLK/2*ADC_CKPS   = 25.0MHz/(1*2) = 12.5MHz  

#define ADC_SHCLK  0xf   // S/H width in ADC module periods                        = 16 ADC clocks  

#define AVG        1000  // Average sample limit  

#define ZOFFSET    0x00  // Average Zero offset  

#define BUF_SIZE   40    // Sample buffer size  

// Global variable for this example  

Uint16 j=0;  

#pragma DATA_SECTION(DMABuf1,"DMARAML4");  

volatile Uint16 DMABuf1[40];  

volatile Uint16 *DMADest;  

volatile Uint16 *DMASource;  

interrupt void local_DINTCH1_ISR(void);  

void main(void)  

{  

  Uint16 i;  

// Step 1. Initialize System Control:  

// PLL, WatchDog, enable Peripheral Clocks  

// This example function is found in the DSP2833x_SysCtrl.c file.  

  InitSysCtrl();  

// Specific clock setting for this example:  

  EALLOW;  

  SysCtrlRegs.HISPCP.all = ADC_MODCLK; // HSPCLK = SYSCLKOUT/ADC_MODCLK  

  EDIS;  

// Step 2. Initialize GPIO:  

// This example function is found in the DSP2833x_Gpio.c file and  

// illustrates how to set the GPIO to it's default state.  

// InitGpio();  // Skipped for this example  

// Step 3. Clear all interrupts and initialize PIE vector table:  

// Disable CPU interrupts  

  DINT;  

// Initialize the PIE control registers to their default state.  

// The default state is all PIE interrupts disabled and flags  

// are cleared.  

// This function is found in the DSP2833x_PieCtrl.c file.  

  InitPieCtrl();  

// Disable CPU interrupts and clear all CPU interrupt flags:  

  IER = 0x0000;  

  IFR = 0x0000;  

// Initialize the PIE vector table with pointers to the shell Interrupt  

// Service Routines (ISR).  

// This will populate the entire table, even if the interrupt  

// is not used in this example.  This is useful for debug purposes.  

// The shell ISR routines are found in DSP2833x_DefaultIsr.c.  

// This function is found in DSP2833x_PieVect.c.  

  InitPieVectTable();  

// Interrupts that are used in this example are re-mapped to  

// ISR functions found within this file.  

  EALLOW;  // Allow access to EALLOW protected registers  

  PieVectTable.DINTCH1= &local_DINTCH1_ISR;  

  EDIS;   // Disable access to EALLOW protected registers  

  IER = M_INT7 ;                                //Enable INT7 (7.1 DMA Ch1)  

  EnableInterrupts();  

// Step 4. Initialize all the Device Peripherals:  

// This function is found in DSP2833x_InitPeripherals.c  

// InitPeripherals(); // Not required for this example  

  InitAdc();  // For this example, init the ADC  

// Specific ADC setup for this example:  

  AdcRegs.ADCTRL1.bit.ACQ_PS = ADC_SHCLK;  

  AdcRegs.ADCTRL3.bit.ADCCLKPS = ADC_CKPS;  

  AdcRegs.ADCTRL1.bit.SEQ_CASC = 0;        // 0 Non-Cascaded Mode  

  AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 0x1;  

  AdcRegs.ADCTRL2.bit.RST_SEQ1 = 0x1;  

  AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;  

  AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1;  

  AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x2;  

  AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x3;  

  AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x0;  

  AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x1;  

  AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x2;  

  AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 0x3;  

  AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 3;   // Set up ADC to perform 4 conversions for every SOC  

//Step 5. User specific code, enable interrupts:  

 // Initialize DMA    

   DMAInitialize();  

   // Clear Table  

  for (i=0; i<BUF_SIZE; i++)  

  {  

    DMABuf1[i] = 0;  

  }  

// Configure DMA Channel  

   DMADest   = &DMABuf1[0];              //Point DMA destination to the beginning of the array  

   DMASource = &AdcMirror.ADCRESULT0;    //Point DMA source to ADC result register base  

   DMACH1AddrConfig(DMADest,DMASource);  

   DMACH1BurstConfig(3,1,10);  

   DMACH1TransferConfig(9,1,0);  

   DMACH1WrapConfig(1,0,0,1);  

   DMACH1ModeConfig(DMA_SEQ1INT,PERINT_ENABLE,ONESHOT_DISABLE,CONT_DISABLE,SYNC_DISABLE,SYNC_SRC,  

                    OVRFLOW_DISABLE,SIXTEEN_BIT,CHINT_END,CHINT_ENABLE);    

   StartDMACH1();  

  // Start SEQ1  

  AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 0x1;  

  for(i=0;i<10;i++){  

       for(j=0;j<1000;j++){}  

       AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;    //Normally ADC will be tied to ePWM, or timed routine  

  }                                         //For this example will re-start manually                      

}  

// INT7.1  

interrupt void local_DINTCH1_ISR(void)     // DMA Channel 1  

{  

 // To receive more interrupts from this PIE group, acknowledge this interrupt    

  PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;  

 // Next two lines for debug only to halt the processor here  

 // Remove after inserting ISR Code  

  asm ("      ESTOP0");  

  for(;;);  

}  

修改后的程序

//###########################################################################  

//  

// FILE:   Example_2833xAdcToDMA.c  

//  

// TITLE:  DSP2833x ADC To DMA  

// ASSUMPTIONS:  

//  

//    This program requires the DSP2833x header files.  

//  

//    Make sure the CPU clock speed is properly defined in  

//    DSP2833x_Examples.h before compiling this example.  

//  

//    Connect the signals to be converted to channel A0, A1, A2, and A3.  

//  

//    As supplied, this project is configured for "boot to SARAM"  

//    operation.  The 2833x Boot Mode table is shown below.  

//    For information on configuring the boot mode of an eZdsp,  

//    please refer to the documentation included with the eZdsp,  

//  

//       $Boot_Table:  

//  

//         GPIO87   GPIO86     GPIO85   GPIO84  

//          XA15     XA14       XA13     XA12  

//           PU       PU         PU       PU  

//        ==========================================  

//            1        1          1        1    Jump to Flash  

//            1        1          1        0    SCI-A boot  

//            1        1          0        1    SPI-A boot  

//            1        1          0        0    I2C-A boot  

//            1        0          1        1    eCAN-A boot  

//            1        0          1        0    McBSP-A boot  

//            1        0          0        1    Jump to XINTF x16  

//            1        0          0        0    Jump to XINTF x32  

//            0        1          1        1    Jump to OTP  

//            0        1          1        0    Parallel GPIO I/O boot  

//            0        1          0        1    Parallel XINTF boot  

//            0        1          0        0    Jump to SARAM       <- "boot to SARAM"  

//            0        0          1        1    Branch to check boot mode  

//            0        0          1        0    Boot to flash, bypass ADC cal  

//            0        0          0        1    Boot to SARAM, bypass ADC cal  

//            0        0          0        0    Boot to SCI-A, bypass ADC cal  

//                                              Boot_Table_End$  

//  

//  

// DESCRIPTION:  

//  

// ADC is setup to convert 4 channels for each SOC received, with  total of 10 SOCs.  

// Each SOC initiates 4 conversions.  

// DMA is set up to capture the data on each SEQ1_INT.  DMA will re-sort      

// the data by channel sequentially, i.e. all channel0 data will be together  

// all channel1 data will be together.  

//  

// Code should stop in local_DINTCH1_ISR when complete  

//  

// Watch Variables:  

//      DMABuf1  

//  

//###########################################################################  

//  

// Original source by: M.P.  

//  

// $TI Release: DSP2833x Header Files V1.10 $  

// $Release Date: February 15, 2008 $  

//###########################################################################  

#include "DSP2833x_Device.h"     // DSP2833x Headerfile Include File  

#include "DSP2833x_Examples.h"   // DSP2833x Examples Include File  

// ADC start parameters  

#if (CPU_FRQ_150MHZ)     // Default - 150 MHz SYSCLKOUT  

 #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3)   = 25.0 MHz  

#endif  

#if (CPU_FRQ_100MHZ)  

 #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2)   = 25.0 MHz  

#endif  

#define ADC_CKPS   0x1   // ADC module clock = HSPCLK/2*ADC_CKPS   = 25.0MHz/(1*2) = 12.5MHz  

#define ADC_SHCLK  0xf   // S/H width in ADC module periods                        = 16 ADC clocks  

#define AVG        1000  // Average sample limit  

#define ZOFFSET    0x00  // Average Zero offset  

#define BUF_SIZE   40    // Sample buffer size  

// Global variable for this example  

Uint16 j=0;  

#pragma DATA_SECTION(DMABuf1,"DMARAML4");  

volatile Uint16 DMABuf1[40];  

volatile Uint16 *DMADest;  

volatile Uint16 *DMASource;  

interrupt void local_DINTCH1_ISR(void);  

void main(void)  

{  

  Uint16 i;  

// Step 1. Initialize System Control:  

// PLL, WatchDog, enable Peripheral Clocks  

// This example function is found in the DSP2833x_SysCtrl.c file.  

  InitSysCtrl();  

// Specific clock setting for this example:  

  EALLOW;  

  SysCtrlRegs.HISPCP.all = ADC_MODCLK; // HSPCLK = SYSCLKOUT/ADC_MODCLK  

  EDIS;  

// Step 2. Initialize GPIO:  

// This example function is found in the DSP2833x_Gpio.c file and  

// illustrates how to set the GPIO to it's default state.  

// InitGpio();  // Skipped for this example  

// Step 3. Clear all interrupts and initialize PIE vector table:  

// Disable CPU interrupts  

  DINT;  

// Initialize the PIE control registers to their default state.  

// The default state is all PIE interrupts disabled and flags  

// are cleared.  

// This function is found in the DSP2833x_PieCtrl.c file.  

  InitPieCtrl();  

// Disable CPU interrupts and clear all CPU interrupt flags:  

  IER = 0x0000;  

  IFR = 0x0000;  

// Initialize the PIE vector table with pointers to the shell Interrupt  

// Service Routines (ISR).  

// This will populate the entire table, even if the interrupt  

// is not used in this example.  This is useful for debug purposes.  

// The shell ISR routines are found in DSP2833x_DefaultIsr.c.  

// This function is found in DSP2833x_PieVect.c.  

  InitPieVectTable();  

// Interrupts that are used in this example are re-mapped to  

// ISR functions found within this file.  

  EALLOW;  // Allow access to EALLOW protected registers  

  PieVectTable.DINTCH1= &local_DINTCH1_ISR;  

  EDIS;   // Disable access to EALLOW protected registers  

  IER = M_INT7 ;                                //Enable INT7 (7.1 DMA Ch1)  

  EnableInterrupts();  

// Step 4. Initialize all the Device Peripherals:  

// This function is found in DSP2833x_InitPeripherals.c  

// InitPeripherals(); // Not required for this example  

  InitAdc();  // For this example, init the ADC  

// Specific ADC setup for this example:  

  AdcRegs.ADCTRL1.bit.ACQ_PS = ADC_SHCLK;  

  AdcRegs.ADCTRL3.bit.ADCCLKPS = ADC_CKPS;  

  AdcRegs.ADCTRL1.bit.SEQ_CASC = 0;        // 0 Non-Cascaded Mode  

  AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 0x1;  

  AdcRegs.ADCTRL2.bit.RST_SEQ1 = 0x1;  

  AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;  

  //AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1;  

  //AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x2;  

  //AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x3;  

  //AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x0;  

  //AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x1;  

  //AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x2;  

  //AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 0x3;  

  AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0;   // Set up ADC to perform 4 conversions for every SOC  

//Step 5. User specific code, enable interrupts:  

 // Initialize DMA    

   DMAInitialize();  

   // Clear Table  

  for (i=0; i<BUF_SIZE; i++)  

  {  

    DMABuf1[i] = 0;  

  }  

// Configure DMA Channel  

   DMADest   = &DMABuf1[0];              //Point DMA destination to the beginning of the array  

   DMASource = &AdcMirror.ADCRESULT0;    //Point DMA source to ADC result register base  

   DMACH1AddrConfig(DMADest,DMASource);  

   DMACH1BurstConfig(0,1,10);  

   DMACH1TransferConfig(9,1,0);  

   DMACH1WrapConfig(1,0,0,1);  

   DMACH1ModeConfig(DMA_SEQ1INT,PERINT_ENABLE,ONESHOT_DISABLE,CONT_DISABLE,SYNC_DISABLE,SYNC_SRC,  

                    OVRFLOW_DISABLE,SIXTEEN_BIT,CHINT_END,CHINT_ENABLE);    

   StartDMACH1();  

  // Start SEQ1  

  AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 0x1;  

  for(i=0;i<10;i++){  

       for(j=0;j<1000;j++){}  

       AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;    //Normally ADC will be tied to ePWM, or timed routine  

  }                                         //For this example will re-start manually                      

}  

// INT7.1  

interrupt void local_DINTCH1_ISR(void)     // DMA Channel 1  

{  

 // To receive more interrupts from this PIE group, acknowledge this interrupt    

  PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;  

 // Next two lines for debug only to halt the processor here  

 // Remove after inserting ISR Code  

  asm ("      ESTOP0");  

  for(;;);  

}

  • 补充说明:我屏蔽掉两个通道,即只采集A0和A1,并在A0口输入正弦波,发现采样回来的波形存在非常大的偏差,但是如果采用原始程序,波形就非常好,请问这是什么原因啊?

  • 请问楼主用的是同步采样么?

    如果同步采样管需要扔掉第一组的数据,具体见F283235的Errata。

  • 我设置的是顺序采样,并且AdcRegs.ADCTRL1.bit.SEQ_CASC = 0;        // 0 Non-Cascaded Mode  ,

    AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;  

    AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0;   // Set up ADC to perform 1 conversions for every SOC

    这样是不是只对对A0进行采样,结果分别放在AdcRegs.ADCRESULT0中?

    然后,我用DMA,配置成

    DMADest   = &DMABuf1[0];              //Point DMA destination to the beginning of the array  

    DMASource = &AdcMirror.ADCRESULT0;    //Point DMA source to ADC result register base  

    DMACH1AddrConfig(DMADest,DMASource);  

    DMACH1BurstConfig(0,1,10);  

    DMACH1TransferConfig(9,1,0);  

    DMACH1WrapConfig(1,0,0,1);  

    这样,把结果放在DMABuf1中。

    运行结果发现,输入的信号是正弦波(采样频率和输入正弦波频率适当),但得到的波形根本不是正弦波。

  • 这样是不是只对对A0进行采样,结果分别放在AdcRegs.ADCRESULT0中?

    是的,SOC0 对应Result0, SOCx 对应 Resultx

    您可以先不用DMA,看看ADC采样的数据是否正确?

  • 请问一下DMA传输的速度到底是不是每个字4个周期啊,为什么下面这个语句要延时那么久,我把j换成100都不能正常工作?

    for(i=0;i<10;i++){  

           for(j=0;j<1000;j++){}  

           AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;    //Normally ADC will be tied to ePWM, or timed routine  

      }                                         //For this example will re-start manually          

  • 还有个问题,就是下面三条语句为什么这样设置?不是应该每1个burst后,源地址都回到起始地址吗?

    DMACH1BurstConfig(3,1,10);

    DMACH1TransferConfig(9,1,0);

    DMACH1WrapConfig(1,0,0,1);每2个burst后,源地址回到起始地址???