Part Number: TMS320F28377D
我的CPU1代码如下
#include "device.h"
#include "F28x_Project.h"
#include "board.h"
#include <driverlib.h>
//
// Defines
//
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
#define Num 10
#pragma DATA_SECTION(readData, "readData")
uint16_t readData[Num];
uint16_t pass;
//IPC通信变量
IPC_MessageQueue_t messageQueue;
IPC_Message_t TxMsg, RxMsg;
/**
* main.c
*/
void main(void)
{
uint32_t i =0 ;
Device_init(); // Initialize device clock and peripherals
Interrupt_initModule(); // Initialize PIE and clear PIE registers. Disables CPU interrupts.
IER = 0x0000; //CPU级中断使能
IFR = 0x0000; //清除CPU级中断标志
Interrupt_initVectorTable(); // Initialize the PIE vector table with pointers to ISR
MemCfg_setGSRAMMasterSel(MEMCFG_SECT_GS13|MEMCFG_SECT_GS14, MEMCFG_GSRAMMASTER_CPU2);
Board_init();
#ifdef _STANDALONE
#ifdef _FLASH
//
// Send boot command to allow the CPU2 application to begin execution
//
Device_bootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
//
// Send boot command to allow the CPU2 application to begin execution
//
Device_bootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif // _FLASH
#endif // _STANDALONE
Device_initGPIO(); // Initialize GPIO and configure the GPIO pin as a push-pull output
//
// Clear any IPC flags if set already
//
IPC_clearFlagLtoR(IPC_CPU1_L_CPU2_R, IPC_FLAG_ALL);
//
// Initialize message queue
//
IPC_initMessageQueue(IPC_CPU1_L_CPU2_R, &messageQueue, IPC_INT1, IPC_INT1);
//
// Synchronize both the cores
//
IPC_sync(IPC_CPU1_L_CPU2_R, SYNC_FLAG);
EINT; // Enable Global Interrupt (INTM)
ERTM; // Enable real-time interrupt (DBGM)
for(i=0; i<Num; i++)
{
readData[i] = i;
}
TxMsg.command = IPC_CMD_READ_MEM;
TxMsg.address = (uint32_t)readData;//强转为uint32_t
TxMsg.dataw1 = Num; // Using dataw1 as data length
TxMsg.dataw2 = 1; // Message identifier
for (;;)
{
GPIO_togglePin(myGPIO99);
DELAY_US(1000000);
//IPC_sendMessageToQueue发送另一个核必须进行读取,否则会出现问题,并且采用非阻塞式发送也会出现问题
//如果是共同的RAM例如GSRAM则不需要校正 否则地址会有偏移
//MSGRAM则需要校正
IPC_sendMessageToQueue(IPC_CPU1_L_CPU2_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE,
&TxMsg, IPC_BLOCKING_CALL);
// IPC_sendCommand(IPC_CPU1_L_CPU2_R,IPC_FLAG1,IPC_ADDR_CORRECTION_DISABLE,0,0,0);
}
}
,我的CPU2代码也在下面#include "device.h"
#include "F28x_Project.h"
#include "board.h"
#include <driverlib.h>
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
#define Num 10
uint16_t readData_CPU2[Num];
uint16_t sendData_CPU2[Num];
#pragma DATA_SECTION(readData_CPU2, "readData_CPU2")
#pragma DATA_SECTION(sendData_CPU2, "sendData_CPU2")
uint16_t IPC_Flag = 0;
uint16_t IPC_Count2 = 0;
bool status = false;
#define myGPIO133 133
IPC_MessageQueue_t messageQueue;
IPC_Message_t TxMsg, RxMsg;
__interrupt void IPC_1_ISR(void);
/**
* main.c
*/
void main(void)
{
Device_init(); // Initialize device clock and peripherals
Device_initGPIO(); // Initialize GPIO and configure the GPIO pin as a push-pull output
Interrupt_initModule(); // Initialize PIE and clear PIE registers. Disables CPU interrupts.
IER = 0x0000; //CPU级中断使能
IFR = 0x0000; //清除CPU级中断标志
Interrupt_initVectorTable(); // Initialize the PIE vector table with pointers to ISR
Board_init();
//
// Clear any IPC flags if set already
//
IPC_clearFlagLtoR(IPC_CPU2_L_CPU1_R, IPC_FLAG_ALL);
//
// Initialize message queue
//
IPC_initMessageQueue(IPC_CPU2_L_CPU1_R, &messageQueue, IPC_INT1, IPC_INT1);
//
// Synchronize both the cores.
//
IPC_sync(IPC_CPU2_L_CPU1_R, SYNC_FLAG);
EINT; // Enable Global Interrupt (INTM)
ERTM; // Enable real-time interrupt (DBGM)
for (;;)
{
;
}
}
__interrupt void IPC_1_ISR(void)
{
uint32_t i;
GPIO_togglePin(myGPIO133);
DELAY_US(1000000);
//
// Read the message from the message queue
//
IPC_readMessageFromQueue(IPC_CPU2_L_CPU1_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE,
&RxMsg, IPC_NONBLOCKING_CALL);
if(RxMsg.command == IPC_CMD_READ_MEM)
{
status = true;
IPC_Count2++;
//
// Read and compare data
//
for(i=0; i<RxMsg.dataw1; i++)
{
if(*((uint16_t *)RxMsg.address + i) != i)//强转为数组类型
status = false;
readData_CPU2[i]=*((uint16_t *)RxMsg.address + i);
sendData_CPU2[i]=readData_CPU2[i]+1;
}
}
// IPC_readCommand(IPC_CPU2_L_CPU1_R,IPC_FLAG1,IPC_ADDR_CORRECTION_DISABLE,0,0,0);
//
// Acknowledge the flag
//
IPC_ackFlagRtoL(IPC_CPU2_L_CPU1_R, IPC_FLAG1);
//
// Acknowledge the PIE interrupt.
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}
现在就是说,调试的时候发现CPU2中断进入了三次,IPC_Count2=3的时候,接下来CPU1就会卡在IPC_sendMessageToQueue函数里面,具体的代码是
while(((writeIndex + 1U) & IPC_MAX_BUFFER_INDEX) == readIndex)
{
// 非阻塞模式直接返回失败
if(!block) {
ret = false;
break;
}
// 阻塞模式下持续更新readIndex等待空间释放
readIndex = *(msgQueue->PutReadIndex);
}
请问是什么原因呢?非常感谢!