Part Number: TMS320F280039C
To synchronize the EPWM counter with the CLB, I am using the CLB to generate a synchronization pulse that is routed via the EPWMXBAR to the EPWM Digital Compare (DC) module. I have some questions now.
1.I noticed that there is a pulse generation section in the DC event triggering part, and I’m not entirely sure how long the pulse width will be.

I routed the DCxEVT1.sync signal to the OUTPUTXBAR and found that the synchronization pulse width is much wider than 1 TBCLK (both SYSCLK and TBCLK are 120 MHz). Is this due to pulse-stretched behavior on EXTSYNCOUT? Will the actual pulse width of DCxEVT.sync be different from the width output to the GPIO?
![]()

2.According to the reference manual, EPWMxSYNCI is activated by rising edge. But what about the signal from the DCxEVT1.sync?
Would a sustained high-level signal cause continuous synchronization?