Other Parts Discussed in Thread: SYSCONFIG
I want to implement two functions :
1. when recieved message identifier is 0x522, generate CAN rx interrupt
2. send DLC = 2~7 can messages,message identifier is 0x521.
3. bit rate is 1Mbps
how to config the CAN module by sysconfig?
when I config the CAN module, I have some doubts:
1. I just use CAN line 0 interrupt, why must I set both CAN interrupt 0 and CAN interrupt 1?
2. What do the options of Flags for Message Object mean? (Enable Transmit interrupts, use filtering base on the Message ID ...)
3. My TX message's length has several different length, should I set several message objects, for example I want send messages length are 2,3,4,5, need I create message object 2,3,4,5 for these different length messages?