Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
您好!
请问:TMS320F28P550SJ使用SysConfig1.23可以同时配置RFFT功能和USB功能吗?能否给出例程。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
您好!
请问:TMS320F28P550SJ使用SysConfig1.23可以同时配置RFFT功能和USB功能吗?能否给出例程。
我使用usb_ex1_dev_serial例程,往里面加入F28P55x_rfft_fpu32例程中的RFFT计算功能,会出现编译不过。反过来使用F28P55x_rfft_fpu32例程,往里面迁移usb_ex1_dev_serial的功能,也会出现编译不过。如下所示:
[75]Building target: "usb_ex1_dev_serial.out"
[76]Invoking: C2000 Linker
[77]"D:/ti/ccs2010/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu1 --vcu_support=vcrc -Ooff --define=RAM --define=ccs_c2k --define=DEBUG --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi -z -m"usb_ex1_dev_serial.map" --heap_size=0x200 --stack_size=0x3F8 --warn_sections -i"D:/ti/ccs2010/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/lib" -i"D:/ti/c2000/C2000Ware_5_04_00_00" -i"C:/Users/lenovo/workspace_ccstheia/usb_ex1_dev_serial/CPU1_RAM/syscfg" -i"D:/ti/ccs2010/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="usb_ex1_dev_serial_linkInfo.xml" --entry_point=code_start --rom_model -o "usb_ex1_dev_serial.out" "./AP_RFFT.obj" "./usb_ex1_dev_serial.obj" "./syscfg/board.obj" "./syscfg/c2000ware_libraries.obj" "./syscfg/usb_structs.obj" "./usb_hal.obj" "./ustdlib.obj" "./device/device.obj" "./device/f28p55x_codestartbranch.obj" "../28p55x_RAM_combined_lnk.cmd" "D:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f28p55x/driverlib/ccs/Debug/driverlib.lib" "D:/ti/c2000/C2000Ware_5_04_00_00/libraries/communications/usb/f28p55x/lib/usblib.lib" -lc2000ware_libraries.cmd.genlibs -llibc.a
[78]<Linking>
[79]warning #10204-D: could not resolve index library "c28x_fpu_dsp_library.lib" to a compatible library
[80] undefined first referenced
[81] symbol in file
[82] --------- ----------------
[83] RFFT_f32_sincostable ./syscfg/c2000ware_libraries.obj
[84]error #10234-D: unresolved symbols remain
[85]error #10010: errors encountered during linking; "usb_ex1_dev_serial.out" not built
[86]>> Compilation failure
[87]makefile:148: recipe for target 'usb_ex1_dev_serial.out' failed
[88]gmake[1]: *** [usb_ex1_dev_serial.out] Error 1
[89]makefile:144: recipe for target 'all' failed
[90]gmake: *** [all] Error 2
[91]**** Build Finished
所以,TMS320F28P550SJ可以同时使用RFFT功能和USB功能吗?