Part Number: TMS320F28034
Other Parts Discussed in Thread: C2000WARE
按照网上的说法,调用了memcpy((uint16_t *)&RamfuncsRunStart,(uint16_t *)&RamfuncsLoadStart, (unsigned long)&RamfuncsLoadSize);
InitFlash();,但是还是进入非法中断
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28034
Other Parts Discussed in Thread: C2000WARE
按照网上的说法,调用了memcpy((uint16_t *)&RamfuncsRunStart,(uint16_t *)&RamfuncsLoadStart, (unsigned long)&RamfuncsLoadSize);
InitFlash();,但是还是进入非法中断
可以参考C2000WARE中的代码进行调试:
例程是有问题的,

//###########################################################################
//
// FILE: Example_2803xAdcSoc.c
//
// TITLE: ADC Start of Conversion example
//
//! \addtogroup f2803x_example_list
//! <h1> ADC Start of Conversion (adc_soc)</h1>
//!
//! This ADC example uses ePWM1 to generate a periodic ADC SOC - ADCINT1.
//! Two channels are converted, ADCINA4 and ADCINA2.
//!
//! \b Watch \b Variables \n
//! - Voltage1[10] - Last 10 ADCRESULT0 values
//! - Voltage2[10] - Last 10 ADCRESULT1 values
//! - ConversionCount - Current result number 0-9
//! - LoopCount - Idle loop counter
//
//
//###########################################################################
// $TI Release: $
// $Release Date: $
// $Copyright:
// Copyright (C) 2009-2025 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//
// Function Prototypes
//
__interrupt void adc_isr(void);
void Adc_Config(void);
//
// Global variables
//
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Voltage1[10];
Uint16 Voltage2[10];
//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2803x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
// InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2803x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize all the Device Peripherals:
//
InitAdc(); // For this example, init the ADC
AdcOffsetSelfCal();
//
// Step 5. User specific code, enable interrupts:
//
//
// Enable ADCINT1 in PIE
//
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
//
// Configure ADC
// Note: Channel ADCINA4 will be double sampled to workaround the
// ADC 1st sample issue for rev0 silicon errata
//
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; // setup EOC2 to trigger
// ADCINT1 to fire
//
// set SOC0 channel select to ADCINA4
// (dummy sample for rev0 errata workaround)
//
AdcRegs.ADCSOC0CTL.bit.CHSEL = 4;
AdcRegs.ADCSOC1CTL.bit.CHSEL = 4; //set SOC1 channel select to ADCINA4
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
//
// set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts
// first then SOC1, then SOC2
//
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5;
//
// set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts
// first then SOC1, then SOC2
//
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5;
//
// set SOC2 start trigger on EPWM1A, due to round-robin SOC0 converts
// first then SOC1, then SOC2
//
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5;
//
// set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;
//
// set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6;
//
// set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6;
EDIS;
//
// Assumes ePWM1 clock is already enabled in InitSysCtrl();
//
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm1Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start
//
// Wait for ADC interrupt
//
for(;;)
{
LoopCount++;
}
}
//
// adc_isr -
//
__interrupt void
adc_isr(void)
{
//
// discard ADCRESULT0 as part of the workaround to the
// 1st sample errata for rev0
//
Voltage1[ConversionCount] = AdcResult.ADCRESULT1;
Voltage2[ConversionCount] = AdcResult.ADCRESULT2;
//
// If 20 conversions have been logged, start over
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
//
// Clear ADCINT1 flag reinitialize for next SOC
//
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
//
// End of File
//
你们也可以跑一下看看,在初始化ADC就会触发非法中断
请尝试参考下面链接,看下能否解决您的问题: