Part Number: TMS320F28P550SJ
亲爱的TI工程师们你们好:
我最近在用TI的28p55 launchpad ,在进行CPU-CLA-DMA测试的时候,为了兼顾CLA和DMA能同时读取ADC结果寄存器的数据,所以将数据放在了 起始地址在0x001700的DMAtoCLA MSG RAM中(cmd文件中为:DMATOCLARAM : origin = 0x001700, length = 0x000080),虽然程序可以正常运行,但是在仿真时就看不到变量了,提示是:Memory map prevented reading 0x00001700@Data,因此想来咨询一下有没有解决方法,谢谢!
我修改后的cmd文件、仿真时遇到的提示信息如下:
CLA_SCRATCHPAD_SIZE = 0x300;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002 // Update the codestart location as needed
BOOT_RSVD : origin = 0x000002, length = 0x000126 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000128, length = 0x0002D8
RAMM1 : origin = 0x000400, length = 0x000400
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMLS8 : origin = 0x014000, length = 0x002000 // When configured as CLA program use the address 0x4000
RAMLS9 : origin = 0x016000, length = 0x002000 // When configured as CLA program use the address 0x6000
//RAMLS8_CLA : origin = 0x004000, length = 0x002000 // Use only if configured as CLA program memory
// RAMLS9_CLA : origin = 0x006000, length = 0x002000 // Use only if configured as CLA program memory
RAMGS0 : origin = 0x00C000, length = 0x002000 //可以DMA访问
RAMGS1 : origin = 0x00E000, length = 0x002000 //可以DMA访问
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x002000 //可以DMA访问
/* Flash Banks (128 sectors each) */
FLASH_BANK0 : origin = 0x080002, length = 0x1FFFE
FLASH_BANK1 : origin = 0x0A0000, length = 0x20000
FLASH_BANK2 : origin = 0x0C0000, length = 0x20000
FLASH_BANK3 : origin = 0x0E0000, length = 0x20000
FLASH_BANK4 : origin = 0x100000, length = 0x07FFF
CLATOCPURAM : origin = 0x001480, length = 0x000080 //CPU和CLA都能访问
CPUTOCLARAM : origin = 0x001500, length = 0x000080 //CPU和CLA都能访问
CLATODMARAM : origin = 0x001680, length = 0x000080 //CPU CLA DMA都能访问
DMATOCLARAM : origin = 0x001700, length = 0x000080 //CPU CLA DMA都能访问
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN
.text : >> FLASH_BANK0 | FLASH_BANK1, ALIGN(8)
.cinit : > FLASH_BANK0, ALIGN(8)
.switch : > FLASH_BANK0, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
.bss : > RAMLS5
.bss:output : > RAMLS3
.init_array : > FLASH_BANK0, ALIGN(8)
.const : > FLASH_BANK0, ALIGN(8)
.data : > RAMLS5 | RAMLS6
.sysmem : > RAMLS4
ramgs0 : > RAMGS0
ramgs1 : > RAMGS1
ramgs2 : > RAMGS2
CLADATARAM :> DMATOCLARAM
// .scratchpad : > RAMLS2
.bss_cla : > RAMLS2
GROUP
{
.TI.ramfunc
ramfuncs
dclfuncs
} LOAD = FLASH_BANK0,
RUN = RAMLS0|RAMLS1,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
GROUP
{
isrcodefuncs
} LOAD = FLASH_BANK1,
RUN = RAMLS3,
LOAD_START(isrcodefuncsLoadStart),
LOAD_SIZE(isrcodefuncsLoadSize),
LOAD_END(isrcodefuncsLoadEnd),
RUN_START(isrcodefuncsRunStart),
RUN_SIZE(isrcodefuncsRunSize),
RUN_END(isrcodefuncsRunEnd),
ALIGN(8)
Cla1Prog : LOAD = FLASH_BANK1,
RUN = RAMLS8,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
ALIGN(4)
.const_cla : LOAD = FLASH_BANK1,
RUN = RAMLS2,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
ALIGN(4)
CLAscratch :
{ *.lib(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.lib(CLAscratch_end) } > RAMLS1
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/

谢谢TI的工程师,还请赐教!