This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的ADC与DMA的问题



菜鸟,初学,求教!

我的在做直流电机控制,ADC采集的是电压。硬件只接了一个ADCINA0。

问题1:ADC采样之后存放在结果寄存器中和存放在DMA中的区别是什么啊?

2:我只有一个采集信号,配置ADC时 ,以下配置可以吗?

 AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0x0;//最大转换通道配置为一个,可以吗?

AdcRegs.ADCCHSELSEQ1.CONV00 = 0x0;

3:对于我这个项目,采集直流电机反馈的电压信号,ADC工作在哪种模式啊?是中断?还是DMA?区别是什么?不理解?

初学,问题幼稚,或者不专业,请大虾指教,谢谢!~