各位大侠:
以前用2.2和3.3烧写F2812片内的FLASH,都是用的插件。那CCS 5.1烧写F2812片内FLASH的方法是什么呢?请大侠们告知!或者能有什么文档可以参考?多谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
直接Load Program就可以,不分Ram和Flash。不用插件。
系统会自动根据CMD文件,来区分是烧写到Ram还是Flash。
建议楼主直接上5.2, 不要纠结于4.x了,就像现在没人装vista系统一样,要装就装win7(CCS5.2),否则就XP(3,3)吧。
关于load 程序,摸索一下,不需要看什么文档。