将matlab里的demo-c2812speedcontrolDC.mdl导入芯片中,没有任何问题。然后,按照help里的指示,连接硬件。从MCU的epwm接到放大器上,在这里我用的是我们实验是的电子版,将MCU的epwm输出口接到电子版块的pwm输入端,然后将直流电机的两极接到电子版块的A,B向上,电子板块要连接一个42伏的电源,然后将解码器的输出口接到QEP1,QEP2的输入口上,在MCU上QEP1和QEP2的引脚就是CAP1,CAP2引脚。其中解码器需要MCU提供一个+5伏的电压,所以我将解码器的+5V的引脚接到了MCU的电源端,这里正好是一个+5V的电压。但是不知道为什么,只要一打开MCU的通电开关,TM320F28335芯片就非常热。请问是什么问题。