This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM320F28335控制直流电机的硬件连接。



将matlab里的demo-c2812speedcontrolDC.mdl导入芯片中,没有任何问题。然后,按照help里的指示,连接硬件。从MCU的epwm接到放大器上,在这里我用的是我们实验是的电子版,将MCU的epwm输出口接到电子版块的pwm输入端,然后将直流电机的两极接到电子版块的A,B向上,电子板块要连接一个42伏的电源,然后将解码器的输出口接到QEP1,QEP2的输入口上,在MCU上QEP1和QEP2的引脚就是CAP1,CAP2引脚。其中解码器需要MCU提供一个+5伏的电压,所以我将解码器的+5V的引脚接到了MCU的电源端,这里正好是一个+5V的电压。但是不知道为什么,只要一打开MCU的通电开关,TM320F28335芯片就非常热。请问是什么问题。

  • 楼主28335是不兼容+5V的,+5V会导致28335烧毁。

    楼主外部是否还有用FPGA,FPGA的引脚设为输出,28335的引脚也为输出的时候,两块芯片都会发烫。

    楼主可以监视一下28335的供电和各个引脚的信号输入信号,如果供电或信号超过3.3V,或者有比较高的毛刺,芯片也会发烫。

    具体的楼主可以参考一下,28335 datasheet的Electrical Specifications,看看哪个信号不符合要求。

  • 请楼主看看Data Sheet, C2000不允许5V输入的。没烧坏芯片已经属于芯片比较皮实了。