This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE: F28P650DK9的SPI部分引脚无法拉高

Part Number: C2000WARE


您好,

我在使用F28P650DK9,封装为169引脚的芯片的引脚55、56、57、58为一组的SPI,在使用中发现读取数据异常,通过示波器抓取发现存在数据波形仅能够拉高至1.3V左右,工程配置如下图:

随后我尝试通过使用GPIO推挽输出高电平的方式将55、58引脚拉高;

结果发现,55引脚能够被拉高至3.3v,58引脚则一直处于低电平;

我们还测试63、64、65、66为一组的SPI以及69、70、71、72的一组SPI,都存在某一个引脚电平拉不起来的情况;

麻烦帮忙测试验证一下;

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    您使用的是C2000WARE SW EX吗?你能运行示例2并告诉我你在示波器上看到了什么吗?您可以尝试不同的GPIO和CLK配置。如果这里没有问题,请分享原始帖子中提到的GPIO配置和示波器图像,并尝试使用示例来帮助配置模块。如果这里有问题,请分享与您的硬件设置相关的信息。

  • 我使用例程spi_ex5_loopback_dma能够实现通信,我将功能复制到自己创建的工程就不好用了,有创建工程的帖子吗?我比对一下看看是不是工程存在问题

  • 您好

    如果可能的话,我会使用spi-ex5_loopback-dma作为启动项目,并在此基础上进行工作(或任何其他spi项目)。最有可能的是,您刚刚错过了复制设置。

    请记住,ex#5不使用任何外部连接,因为SPI在硬件内部触发DMA。示例3确实使用了外部连接,因此您也需要适当的跳线,这可能是您看到的问题的根源,具体取决于您的设置。