This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

从boot 到 app的启动问题



大家好,遇到一个理解不了的问题,还请各位高手帮忙看看

我的是2812处理器,使用的都是片上的资源,我的代码分为两个部分,一部分是boot,另一部分是app,单板启动的时候,首先根据硬件XMP/NMC的配置选择微计算机模式启动,根据GPIO4=1,所以程序跳转到0x3f7ff6运行,而此处放的代码从map文件中看是:

codestart
* 0 003f7ff6 00000002
003f7ff6 00000002 DSP281x_CodeStartBranch.obj (codestart)

这段代码的内容是:

.sect "codestart"

code_start:
.if WD_DISABLE == 1
LB wd_disable ;Branch to watchdog disable code
.else
LB _CheckUserCode ;Branch to start of boot.asm in RTS library
.endif

最后会执行CheckUserCode()函数:

#pragma CODE_SECTION(CheckUserCode,"flashfuncs");
void CheckUserCode(void)
{
if( fcs16(PPPINITFCS16, USER_CODE_START, USER_CODE_LENGTH, CRC_LITTLE_ENDIAN) ==
PPPGOODFCS16 )
{
//goto the User Project Code Start
asm(" LB 0x3F3FFC");
}
{
//goto the Safe project Code Start
SafeModeInitiator = BOOTED_DIRECTLY_TO_SAFE_MODE;
asm(" LB 0x3F7F7E");
}
}

然后根据crc校验去决定 接下来执行boot代码还是跳转到app程序运行。

这是我的板子代码的启动过程,我的问题是如果app程序有改变的时候,是不是crc校验的值就变了呢?那么是否需要更新此校验码?但是奇怪的是我每次改动app后,并没有更新此校验值,但是还是可以跳转到app运行,为什么?