This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
具体信息:
1)自己制作28377D板子,晶振采用外部20MHz时钟,接G19 X1上,通过XDS220仿真器连接DSP成功。
2)使用CCS6.1,版本Version: 6.1.0.00104
3)使用controlSUITE原有工程flash_programming_cpu01。
具体问题:
无法烧写flash。具体提示如下:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU1: File Loader: Verification failed: Values at address 0x0000000000086860 do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\ti\controlSUITE\device_support\F2837xD\v190\F2837xD_examples_Dual\flash_programming\cpu01\ccs\CPU1_FLASH\flash_programming_cpu01.out: a data verification error occurred, file load failed.
您好
如果你是用的TMS开头的量产版芯片请试试先跟新CCS中的烧写插件。具体方法在CCS中点击 help->check for update 然后按提示升级就可以了。
你好,用的是TMS开头的量产芯片。按照check for updata方法,升级过程中会报错,且升级后问题依旧。
烧写插件版本如下:Debug Server Flash 6.1.0.1155 com.ti.dsflash.win32.feature.group Texas Instruments。
我正尝试只升级该烧写插件,看看能不能成功。
另:有没有专门的烧写flahsh插件更新包可以提供,就如同28335一样。
综上,结论:非常感谢 Young Hu & Victor Zheng两位,现在已经可以烧写flash了。
具体操作流程如下:
1、help->About CCS ->Installation Details->Installed Software,搜索flash,点击Debug Server Flash,Update更新即可。
2、一旦更新完成,会提示重启CCS。
3、重启完成之后,Debug Server Flash版本会变成 Debug Server Flash 6.1.0.1425。
4、在Flash Settings也出现可以配置外部时钟、倍频等。