使用2812读取AD芯片转换出的数据,发现2812数据线引脚在程序运行/停止时都是高电平(悬空状态,直接示波器探头观看),这也导致读取到的数据数组全为65535,请问如何配置2812数据线作为输入端,而非一个“电源”输出
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用2812读取AD芯片转换出的数据,发现2812数据线引脚在程序运行/停止时都是高电平(悬空状态,直接示波器探头观看),这也导致读取到的数据数组全为65535,请问如何配置2812数据线作为输入端,而非一个“电源”输出
定义地址:
#define CHA0 0x080022
#define CHA1 0x080026
#define CHB0 0x08002A
#define CHB1 0x08002D
#define CHC0 0x080032
#define CHC1 0x080036
#define CYCLE 0x08003A
#define FIFO 0x08003D
定义通道指针:
ptrCHA0=(int*)CHA0;//通道指针
ptrCHA1=(int*)CHA1;
ptrCHB0=(int*)CHB0;
ptrCHB1=(int*)CHB1;
ptrCHC0=(int*)CHC0;
ptrCHC1=(int*)CHC1;
读取数据的程序:
void read_ADD()
{
CHA0_Data[idxx]=*ptrCHA0;
CHA1_Data[idxx]=*ptrCHA1;
CHB0_Data[idxx]=*ptrCHB0;
CHB1_Data[idxx]=*ptrCHB1;
CHC0_Data[idxx]=*ptrCHC0;
CHC1_Data[idxx]=*ptrCHC1;
idxx=idxx+1;
ADC_ready=1;
if(idxx==Samples)
{
idxx=0;
}
}
没有关于XINTF的配置,程序运行时观察 XRD引脚,可以看到每个周期内有6次低电平,但是就是读入的数据(XD0~XD15)基本都是高,用示波器挑一个数据位观察显示一直为高,这是为什么?