Part Number: TMS320F28P650SH
I need to use the secureboot funciton with CMAC key value 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFE.
I had change the otp 0x7801E to 0xFFFFFFFE .
when the program runs in debug mode, CPU1BROM_calculateCMAC is pass.
but it cannot run in standalone mode.
After the failure in standalone mode, I checked the values of the chip's detection registers, and they match the OTP values.
How can i run the program in standalone mode when the key is set to 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFE?
Btw ,when key is default all F,stand alone mode CPU1BROM_calculateCMAC is pass.