Part Number: TMS320F28P650DK
Hi TI Expert:
I am conducting EtherCAT functional testing on custom hardware. I encountered the following issues:
- I get PDI error in TwinCAT3
- verify ECATPHYCLK failed
How can i close those issues?
The detailed description is as follows:
- my working environment:
- custom hardware based on TMS320F28P650DK7
- C2000Ware5.0.0.0
- CCS 12.5.0.00007
- TwinCAT3 v3.1.4024.62 (Confirm that the network card and software configuration are good.)
- other information:
- TwinCAT3 can scan Box but some information incompleted

- get error EEPROM size and PDI type in TwinCAT3 Smart View

- cant write EEPROM use TwinCAT
- get PDI watchdog cnt in TwinCAT Memory view

- verify XTAL freq 25MHz passed

- verify SYSCLK freq 200MHz passed

- verify ECATPHYCLK freq 100MHz failed, check ECATDIV is 2


- TwinCAT3 can scan Box but some information incompleted
Thanks & Regards