Part Number: TMS320F28335
我用CCS7调试TMS320F28335程序,需要先连接器件才能加载程序。
可是连接期间失败

请高手指教,谢谢
您好,
关于此(Error -1135 @ 0x0)报错请查询此链接中相关章节,software-dl.ti.com/.../ccsv7_debugging_jtag_connectivity_issues.html
This error is commonly associated with C28x devices and is usually associated with a range of hardware or firmware problems that prevent the JTAG debugger to connect to the core.
C28xx: Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error.
Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
The e2e forum threads below cover some possible root causes for this issue:
This error can also manifest when caused by the problems reported in the Invalid data read back section above.
此错误通常与C28x设备相关,通常涉及一系列硬件或固件问题,导致JTAG调试器无法连接到内核。
建议您看看上面的回复的内容以及几个E2E帖子,如果不能解决问题您也可以看看这个链接里有没有和您类似的情况,搜索 - TI E2E 支持论坛