This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 再问编译的问题

Part Number: TMS320F28335

我编译TMS320F28335的程序,出现错误,如下:

谢谢!我改了一下,原来的错误没有了,又出现新的错误。 "C:\Users\chenbingjy\AppData\Local\Temp\0405611", ERROR! at EOF:
[E1500]
file access error: failed to open "E:/Code of TMS320F28335
CCS4/v120/DSP2833x_examples/FFT/Debug/Example_2833x_FFT.obj" for
writing
"C:\Users\chenbingjy\AppData\Local\Temp\0405611", ERROR! : [E1000]
Failed to write object file : E:/Code of TMS320F28335
CCS4/v120/DSP2833x_examples/FFT/Debug/Example_2833x_FFT.obj >> Compilation failure
C:\ti\ccsv4\utils\gmake\gmake: *** [E:/Code of TMS320F28335 CCS4/v120/DSP2833x_examples/FFT/Debug/Example_2833x_FFT.obj] Error 1
C:\ti\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.
Build complete for project EXT_ROOT__Example_2833x_FFT

我的工程在D盘,编译结果错误显示在E盘。

这个问题怎么解决?谢谢