This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

移植Flash2812_API_V210.lib报警告no matching section

问题描述,在CMD中将Flash2812_API_V210.lib定义到RAM里,结果一直报这个警告说:no matching section然后指向这两行

但实际我已经将Flash2812_API_V210.lib添加进来了

有没有大神给解决下问题

  • 是不是路径包含的问题引起的呢?

  • 按说这样添加进来就好了吧

  • 附上我的CMD文件
    MEMORY
    {
    PAGE 0: /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

    ZONE0 : origin = 0x002000, length = 0x002000 /* XINTF zone 0 */
    ZONE1 : origin = 0x004000, length = 0x002000 /* XINTF zone 1 */
    RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
    RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
    ZONE2 : origin = 0x080000, length = 0x080000 /* XINTF zone 2 */
    ZONE6 : origin = 0x100000, length = 0x080000 /* XINTF zone 6 */
    OTP : origin = 0x3D7800, length = 0x000800 /* on-chip OTP */
    FLASHJ : origin = 0x3D8000, length = 0x002000 /* on-chip FLASH */
    FLASHI : origin = 0x3DA000, length = 0x002000 /* on-chip FLASH */
    FLASHH : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
    FLASHG : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
    FLASHF : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
    FLASHE : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
    FLASHD : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
    FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
    FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
    FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
    /* ZONE7 : origin = 0x3FC000, length = 0x003FC0 /* XINTF zone 7 available if MP/MCn=1 */
    ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM available if MP/MCn=0 */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */
    }

    SECTIONS
    {

    codestart : > BEGIN, PAGE = 0

    ramfuncs : LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0
    Flash28_API:
    {
    -lFlash2812_API_V210.lib(.econst)
    -lFlash2812_API_V210.lib(.text)
    } LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_Flash28_API_LoadStart),
    LOAD_END(_Flash28_API_LoadEnd),
    RUN_START(_Flash28_API_RunStart),
    PAGE = 0


    csmpasswds : > CSM_PWL PAGE = 0
    csm_rsvd : > CSM_RSVD PAGE = 0
    .text : > FLASHA, PAGE = 0
    .cinit : > FLASHA, PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .switch : > FLASHA, PAGE = 0
    .reset : > RESET, PAGE = 0, TYPE = DSECT

    IQmathTables : load = ROM, type = NOLOAD, PAGE = 0
    IQmath : load =FLASHC, PAGE = 0
    FFTtf : > FLASHA, PAGE = 0
    SINTBL : > FLASHA, PAGE = 0
    .econst : > FLASHA, PAGE = 0
    iirfilt : > RAML1, PAGE = 0
    FFTipcb1 : > RAML1, PAGE = 0

    .stack : > RAMM1, PAGE = 1
    .ebss : > RAMH0, PAGE = 1
    }