This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335外部中断总结



在这里我们要十分清楚DSP的中断系统。C28XX一共有16个中断源,其中有2个不可屏蔽的中断RESET和NMI、定时器1和定时器2分别使用中断13  
和14。这样还有12个中断都直接连接到外设中断扩展模块PIE上。说的简单一点就是PIE通过12根线与28335核的12个中断线相连。而PIE的另外  
一侧有12*8根线分别连接到外设,如AD、SPI、EXINT等等。这样PIE共管理12*8=96个外部中断。这12组大中断由28335核的中断寄存器IER来控  
制,即IER确定每个中断到底属于哪一组大中断(如IER |= M_INT12;说明我们要用第12组的中断,但是第12组里面的什么中断CPU并不知道需  
要再由PIEIER确定)。接下来再由PIE模块中的寄存器PIEIER中的低8确定该中断是这一组的第几个中断,这些配置都要告诉CPU(我们不难想  
象到PIEIER共有12总即从PIEIER1-PIEIER12)。另外,PIE模块还有中断标志寄存器PIEIFR,同样它的低8位是来自外部中断的8个标志位,同  
样CPU的IFR寄存器是中断组的标志寄存器。由此看来,CPU的所有中断寄存器控制12组的中断,PIE的所有中断寄存器控制每组内8个的中断。  
除此之外,我们用到哪一个外部中断,相应的还有外部中断的寄存器,需要注意的就是外部中断的标志要自己通过软件来清零。而PIE和CPU的  
中断标志寄存器由硬件来清零。   
    EALLOW;  // This is needed to write to EALLOW protected registers   
   PieVectTable.XINT2 = &ISRExint; //告诉中断入口地址  
   EDIS;    // This is needed to disable write to EALLOW protected registers    
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;          // Enable the PIE block使能PIE  
    PieCtrlRegs.PIEIER1.bit.INTx5= 1;   //使能第一组中的中断5  
   IER |= M_INT1;                              // Enable CPU 第一组中断

EINT;   // Enable Global interrupt INTM  
    ERTM;   // Enable Global realtime interrupt DBGM    
也就是说,12组中的每个中断都要完成上面的相同配置,剩下的才是去配置自己的中断。如我们提到的EXINT,即外面来个低电平我们就进入  
中断,完成我们的程序。在这里要介绍一下,DSP的GPIO口都可以配置为外部中断口,其配置方法如下:  
     GpioCtrlRegs.GPBMUX2.bit.GPIO54 = 0; //选择他们是GPIO口  
     GpioCtrlRegs.GPBMUX2.bit.GPIO55 = 0;  
     GpioCtrlRegs.GPBMUX2.bit.GPIO56 = 0;  
     GpioCtrlRegs.GPBMUX2.bit.GPIO57 = 0;  
     GpioCtrlRegs.GPBDIR.bit.GPIO54 = 0;//选择他们都是输入口  
     GpioCtrlRegs.GPBDIR.bit.GPIO55 = 0;  
     GpioCtrlRegs.GPBDIR.bit.GPIO56 = 0;  
     GpioCtrlRegs.GPBDIR.bit.GPIO57 = 0;  
     GpioCtrlRegs.GPBQSEL2.bit.GPIO54= 0;//GPIO时钟和系统时钟一样且支持GPIO  
     GpioCtrlRegs.GPBQSEL2.bit.GPIO55= 0;  
     GpioCtrlRegs.GPBQSEL2.bit.GPIO56= 0;  
     GpioCtrlRegs.GPBQSEL2.bit.GPIO57= 0;  
     GpioIntRegs.GPIOXINT3SEL.bit.GPIOSEL = 54;//中断3选择GPIO  
     GpioIntRegs.GPIOXINT4SEL.bit.GPIOSEL = 55;  
     GpioIntRegs.GPIOXINT5SEL.bit.GPIOSEL = 56;  
     GpioIntRegs.GPIOXINT6SEL.bit.GPIOSEL = 57;

XIntruptRegs.XINT3CR.bit.POLARITY= 0;//触发模式为下降沿触发  
     XIntruptRegs.XINT4CR.bit.POLARITY= 0;  
     XIntruptRegs.XINT5CR.bit.POLARITY= 0;  
     XIntruptRegs.XINT6CR.bit.POLARITY= 0;  
     XIntruptRegs.XINT3CR.bit.ENABLE = 1;//使能中断  
     XIntruptRegs.XINT4CR.bit.ENABLE = 1;  
     XIntruptRegs.XINT5CR.bit.ENABLE = 1;  
     XIntruptRegs.XINT6CR.bit.ENABLE = 1;  
注意一点就是外部中断1和2只能对GPIO0—GPIO31配置;外部中断3和4、5、6、7只对GPIO32—GPIO63配置。