This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28335官方移植里对RTOS中断处理的说明,
任务级和中断级的切换机制怎么变成一样的了?
官方指的是TI的合作商Micrium公司,移植文件指的是Micrium公司为TMDSDOCK28335 (TMS320F28335) evaluation board提供的ucos操作系统移植文件,文件名为:Micrium_TMDSDOCK28335_OS2.zip从https://www.micrium.com/网站可以下载。我的问题出自移植文件os_cpu_a.asm,不知道这次表述是否够清晰。以下为文件全文,非常感谢。
;
;********************************************************************************************************
; uC/OS-II
; The Real-Time Kernel
;
;
; (c) Copyright 2009-2015; Micrium, Inc.; Weston, FL
; All rights reserved. Protected by international copyright laws.
;
; TI C28x Port
;
; File : OS_CPU_A.ASM
; Version : V2.92.11
; By : JFT
;
; LICENSING TERMS:
; ---------------
; uC/OS-II is provided in source form for FREE short-term evaluation, for educational use or
; for peaceful research. If you plan or intend to use uC/OS-II in a commercial application/
; product then, you need to contact Micrium to properly license uC/OS-II for its use in your
; application/product. We provide ALL the source code for your convenience and to help you
; experience uC/OS-II. The fact that the source is provided does NOT mean that you can use
; it commercially without paying a licensing fee.
;
; Knowledge of the source code may NOT be used to develop a similar product.
;
; Please help us continue to provide the embedded community with the finest software available.
; Your honesty is greatly appreciated.
;
; You can contact us at www.micrium.com, or by phone at +1 (954) 217-2036.
;
; For : TI C28x
; Mode : C28 Object mode
; Toolchain : TI C/C++ Compiler
;********************************************************************************************************
;
;********************************************************************************************************
; INCLUDE FILES
;********************************************************************************************************
.include "os_cpu_i.asm"
;********************************************************************************************************
; EXTERNAL GLOBAL VARIABLES
;********************************************************************************************************
; External references
.ref _OSRunning
.ref _OSPrioCur
.ref _OSPrioHighRdy
.ref _OSTCBCur
.ref _OSTCBHighRdy
.ref _OSIntExit
.ref _OSTaskSwHook
;********************************************************************************************************
; PUBLIC FUNCTIONS
;********************************************************************************************************
; Functions declared in this file
.def _OS_CPU_GetST0
.def _OS_CPU_GetST1
.def _OS_CPU_SR_Save
.def _OS_CPU_SR_Restore
.def _OSStartHighRdy
.def _OS_CPU_RTOSINT_Handler
;********************************************************************************************************
; EQUATES
;********************************************************************************************************
;********************************************************************************************************
; CODE GENERATION DIRECTIVES
;********************************************************************************************************
; Set text section and reset local labels.
.text
.newblock
;********************************************************************************************************
; GET ST0 and ST1
;
; Description : Wrapper function to get ST0 and ST1 registers from a C function.
;
; Prototypes : INT16U OS_CPU_GetST0(void);
; INT16U OS_CPU_GetST1(void);
;********************************************************************************************************
.asmfunc
_OS_CPU_GetST0:
PUSH ST0
POP AL
LRETR
.endasmfunc
.asmfunc
_OS_CPU_GetST1:
PUSH ST1
POP AL
LRETR
.endasmfunc
;********************************************************************************************************
; CRITICAL SECTION METHOD 3 FUNCTIONS
;
; Description: Disable/Enable interrupts by preserving the state of interrupts. Generally speaking you
; would store the state of the interrupt disable flag in the local variable 'cpu_sr' and then
; disable interrupts. 'cpu_sr' is allocated in all of uC/OS-II's functions that need to
; disable interrupts. You would restore the interrupt disable state by copying back 'cpu_sr'
; into the CPU's status register.
;
; Prototypes : OS_CPU_SR OS_CPU_SR_Save(void);
; void OS_CPU_SR_Restore(OS_CPU_SR cpu_sr);
;
;
; Note(s) : 1) These functions are used in general like this:
;
; void Task (void *p_arg)
; {
; #if OS_CRITICAL_METHOD == 3 /* Allocate storage for CPU status register */
; OS_CPU_SR cpu_sr;
; #endif
;
; :
; :
; OS_ENTER_CRITICAL(); /* cpu_sr = OS_CPU_SaveSR(); */
; :
; :
; OS_EXIT_CRITICAL(); /* OS_CPU_RestoreSR(cpu_sr); */
; :
; :
; }
;********************************************************************************************************
.asmfunc
_OS_CPU_SR_Save:
PUSH ST1
DINT
POP @AL
AND AL, #1
LRETR
.endasmfunc
.asmfunc
_OS_CPU_SR_Restore:
PUSH ST1
POP AR0
AND AR0, #0xFFFE
OR AL, AR0
PUSH AL
POP ST1
LRETR
.endasmfunc
;********************************************************************************************************
; START MULTITASKING
; void OSStartHighRdy(void)
; Note(s) : 1) This function triggers a PendSV exception (essentially, causes a context switch) to cause
; the first task to start.
;
; 2) OSStartHighRdy() MUST:
; a) Call OSTaskSwHook().
; b) Set OSRunning to TRUE;
; c) Restore context for OSTCBCurPtr.
; d) IRET into highest ready task.
;********************************************************************************************************
.asmfunc
_OSStartHighRdy:
; Call OSTaskSwHook()
LCR #_OSTaskSwHook
; Set OSRunning to TRUE.
MOVL XAR0, #_OSRunning
MOV *AR0, #1
; Restore context.
MOVL XAR0, #_OSTCBCur ; Get the process's SP.
MOVL XAR1, *XAR0
MOV AL , *AR1
MOV @SP , AL
; Restore registers.
OS_CTX_RESTORE
; IRET into task.
IRET
.endasmfunc
; Catch start high failure.
OSStartHang:
SB OSStartHang, UNC
;********************************************************************************************************
; HANDLE RTOSINT INTERRUPT
; void OS_CPU_RTOSINT_Handler(void)
;
; Note(s) : 1) The RTOSINT interrupt is used to perform a context switch. The C28x core saves the
; ST0, T, ACC, P, AR0, AR1, ST1, DP, IER, DBGSTAT (shadow) registers and the Return
; Address.
; The remaining registers AR1H, AR0H, XAR2..XAR7, XT and RPC are saved by the handler.
; Using RTOSINT means that the switching mechanism is the same for a task or an ISR.
; 2) The context switching RTOSINT handler pseudo-code is:
; a) Save remaining registers on the process stack;
; b) Save the process SP in its TCB, OSTCBCurPtr->OSTCBStkPtr = SP;
; c) Call OSTaskSwHook();
; d) Get current high priority, OSPrioCur = OSPrioHighRdy;
; e) Get current ready thread TCB, OSTCBCur = OSTCBHighRdy;
; f) Get new process SP from TCB, SP = OSTCBHighRdy->OSTCBStkPtr;
; g) Restore AR1H, AR0H, XAR2..XAR7, XT and RPC registers from the new process stack;
; h) Overwrite the previously saved (at context switch out) IER register with current IER.
; i) Perform exception return which will restore remaining context.
;
; 3) On entry into RTOSINT handler:
; a) The following have been saved on the process stack (by processor):
; ST0, T, ACC, P, AR0, AR1, ST1, DP, IER, DBGSTAT (shadow) registers and the Return
; Address.
; b) OSTCBCurPtr points to the OS_TCB of the task to suspend
; OSTCBHighRdyPtr points to the OS_TCB of the task to resume
;
; 4) This function MUST be placed in entry 16 (for RTOSINT) of the C28x interrupt table.
;********************************************************************************************************
.asmfunc
_OS_CPU_RTOSINT_Handler:
; Save registers.
OS_CTX_SAVE
; Save SP to current process.
MOVL XAR0, #_OSTCBCur ; Get the process's SP.
MOVL XAR1, *XAR0
MOV AL , @SP
MOV *AR1, AL
ASP ; Align the stack pointer.
; Call OSTaskSwHook.
LCR #_OSTaskSwHook
NASP ; Restore alignement of the stack pointer.
; OSPrioCur = OSPrioHighRdy
MOVL XAR0, #_OSPrioHighRdy
MOVL XAR1, #_OSPrioCur
MOV ACC, *XAR0
MOV *XAR1, ACC
; OSTCBCur = OSTCBHighRdy
MOVL XAR0, #_OSTCBHighRdy
MOVL XAR1, #_OSTCBCur
MOVL ACC, *XAR0
MOVL *XAR1, ACC
; Get SP from new process.
MOVL XAR0, *XAR1
MOV AL , *AR0
MOV @SP , AL
OS_CTX_RESTORE
; Return from interrupt to restore remaining registers.
IRET
.endasmfunc
;********************************************************************************************************
; OS-II ASSEMBLY PORT FILE END
;********************************************************************************************************
.end
它的描述应该是使用RTOSINT来实现上下文的切换,进行现场保护,采用了与任务类似的处理方式,并不一定是相同的优先级。
这个代码与TI没有任何关系,只是第三方使用TI的硬件来运行它们的代码,所以更详细的解释或说明,还请与他们直接联系。