This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335官方移植ucos疑惑

Other Parts Discussed in Thread: TMS320F28335, TMDSDOCK28335

28335官方移植里对RTOS中断处理的说明,
任务级和中断级的切换机制怎么变成一样的了?

  • "官方移植"是哪里的出处?能不能提供完整的路径或截图说明,让别人能够容易找到,才方便更快解决你的问题。

  • 官方指的是TI的合作商Micrium公司,移植文件指的是Micrium公司为TMDSDOCK28335 (TMS320F28335) evaluation board提供的ucos操作系统移植文件,文件名为:Micrium_TMDSDOCK28335_OS2.zip从https://www.micrium.com/网站可以下载。我的问题出自移植文件os_cpu_a.asm,不知道这次表述是否够清晰。以下为文件全文,非常感谢。

    ;
    ;********************************************************************************************************
    ; uC/OS-II
    ; The Real-Time Kernel
    ;
    ;
    ; (c) Copyright 2009-2015; Micrium, Inc.; Weston, FL
    ; All rights reserved. Protected by international copyright laws.
    ;
    ; TI C28x Port
    ;
    ; File : OS_CPU_A.ASM
    ; Version : V2.92.11
    ; By : JFT
    ;
    ; LICENSING TERMS:
    ; ---------------
    ; uC/OS-II is provided in source form for FREE short-term evaluation, for educational use or
    ; for peaceful research. If you plan or intend to use uC/OS-II in a commercial application/
    ; product then, you need to contact Micrium to properly license uC/OS-II for its use in your
    ; application/product. We provide ALL the source code for your convenience and to help you
    ; experience uC/OS-II. The fact that the source is provided does NOT mean that you can use
    ; it commercially without paying a licensing fee.
    ;
    ; Knowledge of the source code may NOT be used to develop a similar product.
    ;
    ; Please help us continue to provide the embedded community with the finest software available.
    ; Your honesty is greatly appreciated.
    ;
    ; You can contact us at www.micrium.com, or by phone at +1 (954) 217-2036.
    ;
    ; For : TI C28x
    ; Mode : C28 Object mode
    ; Toolchain : TI C/C++ Compiler
    ;********************************************************************************************************
    ;

    ;********************************************************************************************************
    ; INCLUDE FILES
    ;********************************************************************************************************

    .include "os_cpu_i.asm"


    ;********************************************************************************************************
    ; EXTERNAL GLOBAL VARIABLES
    ;********************************************************************************************************
    ; External references
    .ref _OSRunning
    .ref _OSPrioCur
    .ref _OSPrioHighRdy
    .ref _OSTCBCur
    .ref _OSTCBHighRdy
    .ref _OSIntExit
    .ref _OSTaskSwHook


    ;********************************************************************************************************
    ; PUBLIC FUNCTIONS
    ;********************************************************************************************************
    ; Functions declared in this file
    .def _OS_CPU_GetST0
    .def _OS_CPU_GetST1
    .def _OS_CPU_SR_Save
    .def _OS_CPU_SR_Restore
    .def _OSStartHighRdy
    .def _OS_CPU_RTOSINT_Handler


    ;********************************************************************************************************
    ; EQUATES
    ;********************************************************************************************************


    ;********************************************************************************************************
    ; CODE GENERATION DIRECTIVES
    ;********************************************************************************************************
    ; Set text section and reset local labels.
    .text
    .newblock


    ;********************************************************************************************************
    ; GET ST0 and ST1
    ;
    ; Description : Wrapper function to get ST0 and ST1 registers from a C function.
    ;
    ; Prototypes : INT16U OS_CPU_GetST0(void);
    ; INT16U OS_CPU_GetST1(void);
    ;********************************************************************************************************

    .asmfunc
    _OS_CPU_GetST0:
    PUSH ST0
    POP AL
    LRETR
    .endasmfunc

    .asmfunc
    _OS_CPU_GetST1:
    PUSH ST1
    POP AL
    LRETR
    .endasmfunc


    ;********************************************************************************************************
    ; CRITICAL SECTION METHOD 3 FUNCTIONS
    ;
    ; Description: Disable/Enable interrupts by preserving the state of interrupts. Generally speaking you
    ; would store the state of the interrupt disable flag in the local variable 'cpu_sr' and then
    ; disable interrupts. 'cpu_sr' is allocated in all of uC/OS-II's functions that need to
    ; disable interrupts. You would restore the interrupt disable state by copying back 'cpu_sr'
    ; into the CPU's status register.
    ;
    ; Prototypes : OS_CPU_SR OS_CPU_SR_Save(void);
    ; void OS_CPU_SR_Restore(OS_CPU_SR cpu_sr);
    ;
    ;
    ; Note(s) : 1) These functions are used in general like this:
    ;
    ; void Task (void *p_arg)
    ; {
    ; #if OS_CRITICAL_METHOD == 3 /* Allocate storage for CPU status register */
    ; OS_CPU_SR cpu_sr;
    ; #endif
    ;
    ; :
    ; :
    ; OS_ENTER_CRITICAL(); /* cpu_sr = OS_CPU_SaveSR(); */
    ; :
    ; :
    ; OS_EXIT_CRITICAL(); /* OS_CPU_RestoreSR(cpu_sr); */
    ; :
    ; :
    ; }
    ;********************************************************************************************************

    .asmfunc
    _OS_CPU_SR_Save:
    PUSH ST1
    DINT
    POP @AL
    AND AL, #1
    LRETR
    .endasmfunc

    .asmfunc
    _OS_CPU_SR_Restore:
    PUSH ST1
    POP AR0
    AND AR0, #0xFFFE
    OR AL, AR0
    PUSH AL
    POP ST1
    LRETR
    .endasmfunc


    ;********************************************************************************************************
    ; START MULTITASKING
    ; void OSStartHighRdy(void)
    ; Note(s) : 1) This function triggers a PendSV exception (essentially, causes a context switch) to cause
    ; the first task to start.
    ;
    ; 2) OSStartHighRdy() MUST:
    ; a) Call OSTaskSwHook().
    ; b) Set OSRunning to TRUE;
    ; c) Restore context for OSTCBCurPtr.
    ; d) IRET into highest ready task.
    ;********************************************************************************************************
    .asmfunc
    _OSStartHighRdy:
    ; Call OSTaskSwHook()
    LCR #_OSTaskSwHook
    ; Set OSRunning to TRUE.
    MOVL XAR0, #_OSRunning
    MOV *AR0, #1
    ; Restore context.
    MOVL XAR0, #_OSTCBCur ; Get the process's SP.
    MOVL XAR1, *XAR0
    MOV AL , *AR1
    MOV @SP , AL
    ; Restore registers.
    OS_CTX_RESTORE
    ; IRET into task.
    IRET
    .endasmfunc
    ; Catch start high failure.
    OSStartHang:
    SB OSStartHang, UNC


    ;********************************************************************************************************
    ; HANDLE RTOSINT INTERRUPT
    ; void OS_CPU_RTOSINT_Handler(void)
    ;
    ; Note(s) : 1) The RTOSINT interrupt is used to perform a context switch. The C28x core saves the
    ; ST0, T, ACC, P, AR0, AR1, ST1, DP, IER, DBGSTAT (shadow) registers and the Return
    ; Address.
    ; The remaining registers AR1H, AR0H, XAR2..XAR7, XT and RPC are saved by the handler.
    ; Using RTOSINT means that the switching mechanism is the same for a task or an ISR.

    ; 2) The context switching RTOSINT handler pseudo-code is:
    ; a) Save remaining registers on the process stack;
    ; b) Save the process SP in its TCB, OSTCBCurPtr->OSTCBStkPtr = SP;
    ; c) Call OSTaskSwHook();
    ; d) Get current high priority, OSPrioCur = OSPrioHighRdy;
    ; e) Get current ready thread TCB, OSTCBCur = OSTCBHighRdy;
    ; f) Get new process SP from TCB, SP = OSTCBHighRdy->OSTCBStkPtr;
    ; g) Restore AR1H, AR0H, XAR2..XAR7, XT and RPC registers from the new process stack;
    ; h) Overwrite the previously saved (at context switch out) IER register with current IER.
    ; i) Perform exception return which will restore remaining context.
    ;
    ; 3) On entry into RTOSINT handler:
    ; a) The following have been saved on the process stack (by processor):
    ; ST0, T, ACC, P, AR0, AR1, ST1, DP, IER, DBGSTAT (shadow) registers and the Return
    ; Address.
    ; b) OSTCBCurPtr points to the OS_TCB of the task to suspend
    ; OSTCBHighRdyPtr points to the OS_TCB of the task to resume
    ;
    ; 4) This function MUST be placed in entry 16 (for RTOSINT) of the C28x interrupt table.
    ;********************************************************************************************************

    .asmfunc
    _OS_CPU_RTOSINT_Handler:
    ; Save registers.
    OS_CTX_SAVE
    ; Save SP to current process.
    MOVL XAR0, #_OSTCBCur ; Get the process's SP.
    MOVL XAR1, *XAR0
    MOV AL , @SP
    MOV *AR1, AL

    ASP ; Align the stack pointer.
    ; Call OSTaskSwHook.
    LCR #_OSTaskSwHook
    NASP ; Restore alignement of the stack pointer.

    ; OSPrioCur = OSPrioHighRdy
    MOVL XAR0, #_OSPrioHighRdy
    MOVL XAR1, #_OSPrioCur
    MOV ACC, *XAR0
    MOV *XAR1, ACC
    ; OSTCBCur = OSTCBHighRdy
    MOVL XAR0, #_OSTCBHighRdy
    MOVL XAR1, #_OSTCBCur
    MOVL ACC, *XAR0
    MOVL *XAR1, ACC
    ; Get SP from new process.
    MOVL XAR0, *XAR1
    MOV AL , *AR0
    MOV @SP , AL

    OS_CTX_RESTORE
    ; Return from interrupt to restore remaining registers.
    IRET
    .endasmfunc


    ;********************************************************************************************************
    ; OS-II ASSEMBLY PORT FILE END
    ;********************************************************************************************************

    .end

  • 它的描述应该是使用RTOSINT来实现上下文的切换,进行现场保护,采用了与任务类似的处理方式,并不一定是相同的优先级。

    这个代码与TI没有任何关系,只是第三方使用TI的硬件来运行它们的代码,所以更详细的解释或说明,还请与他们直接联系。

  • RTOSINT机制和其他CPU中断的机制没有什么不同吧?

  • 没有,就是正常的中断,它这里只是描述了C28x在进入中断时都会做的动作,即保存哪些CPU寄存器。

  • 这个似乎和现场保护,只是说28335可以通过中断方式处理任务切换,那么现场保护由中断机制自动完成,好多低端的U并没有这个能力,比如51,就必须手工进行现场保护.

  • 您好,能不能发一份儿官方的28335的ucos代码给我。我在micrium注册了好久,都收不到激活邮件,所以也不能下载。谢谢!邮箱799612119@qq.com

  • 你好,请问可以提供一份官方的ucosii移植在28335上的源代码吗?最近正在学习DSP上的实时操作系统。邮箱:820307266@qq.com,谢谢