This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035的ADC单触发源触发转换怎么理解呢?



       各位老师好,我学习DSP28035的时候有这样一句话:    “每一个SOC 都是独立配置的,并且可以有触发源,通道和采样时间的任意组合。这就提供了一种灵活的方式来配置转换,包括用不同的触发源分别采样不同的通道,使用单一的触发源过采样相同的通道和创建用单一的触发源触发一系列不同的通道。”怎样理解这句话呢??

  • SOC可以理解为一个内部事件,这个事件决定了转换和采样的优先级,而这个事件可以独立配置到任意外部ADC引脚,以及配置自己的采样窗宽度,和被触发采样的触发源。所以会相对F28335的顺序触发采样灵活,也就是你可以理解为每个采样通道都可以通过SOC的配置变成任意优先级。并且通过不同的触发源配置可以控制不同的采样周期。