This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何给C2000的CPU定时器分频



       请问为什么我把CpuTimer2Regs.TPR.bit.PSC设置为某个值比如10不能对CPU定时器2进行分频,结果出来完全没有分频效果,而把CpuTimer2Regs.TPRH.bit.PSC设置为某个值却能对CPU定时器2进行有效分频,结果是对的

  • 请注意,PSC和PSCH本来就是只读位,设置分频应该从TDDR和TDDRH位来设置

    CPU-Timer Prescale Counter. These bits hold the current prescale count for the timer. For every timer clock
    source cycle that the PSCH:PSC value is greater than 0, the PSCH:PSC decrements by one. One timer clock
    (output of the timer prescaler) cycle after the PSCH:PSC reaches 0, the PSCH:PSC is loaded with the contents
    of the TDDRH:TDDR, and the timer counter register (TIMH:TIM) decrements by one. The PSCH:PSC is also
    reloaded whenever the timer reload bit (TRB) is set by software. The PSCH:PSC can be checked by reading
    the register, but it cannot be set directly. It must get its value from the timer divide-down register
    (TDDRH:TDDR). At reset, the PSCH:PSC is set to 0.

    PSC的解释,这只是一个active寄存器的分频值,每次减到0后,让timer clock输出一次,然后把TDDR/TDDRH的值load到PSC/PSCH一次。这是他的工作原理,所以TDDR/TDDRH可以视为shadow寄存器,每次更新后,要等到当次PSC/PSCH减到0才会从新load。下面是TDDR/TDDRH的解释:

    CPU-Timer Prescale Counter. These bits hold the current prescale count for the timer. For every timer clock
    source cycle that the PSCH:PSC value is greater than 0, the PSCH:PSC decrements by one. One timer clock
    (output of the timer prescaler) cycle after the PSCH:PSC reaches 0, the PSCH:PSC is loaded with the contents
    of the TDDRH:TDDR, and the timer counter register (TIMH:TIM) decrements by one. The PSCH:PSC is also
    reloaded whenever the timer reload bit (TRB) is set by software. The PSCH:PSC can be checked by reading
    the register, but it cannot be set directly. It must get its value from the timer divide-down register
    (TDDRH:TDDR). At reset, the PSCH:PSC is set to 0.