This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

flash_kernel例程的_InitBoot:_ExitBoot不解

下面  LCR  _main运行完后,EntryAddr不是应该放在RPC里吗,为何在ACC里?PUSH ACC, POP  RPC又是何意?

_InitBoot:

; Initalize the stack pointer.

__stack:    .usect ".stack",0
    MOV SP, #__stack ; Initalize the stack pointer

; Initalize the device for running in C28x mode.

    C28OBJ       ; Select C28x object mode
    C28ADDR      ; Select C27x/C28x addressing
    C28MAP       ; Set blocks M0/M1 for C28x mode
    CLRC PAGE0   ; Always use stack addressing mode
    MOVW DP,#0   ; Initialize DP to point to the low 64 K
    CLRC OVM

; Set PM shift of 0

    SPM 0

; Decide which boot mode to use
    LCR  _main

; Cleanup and exit.  At this point the EntryAddr
; is located in the ACC register
    BF  _ExitBoot,UNC

 

;-----------------------------------------------
; _ExitBoot
;-----------------------------------------------
;-----------------------------------------------
;This module cleans up after the boot loader
;
; 1) Make sure the stack is deallocated.
;    SP = 0x400 after exiting the boot
;    loader
; 2) Push 0 onto the stack so RPC will be
;    0 after using LRETR to jump to the
;    entry point
; 2) Load RPC with the entry point
; 3) Clear all XARn registers
; 4) Clear ACC, P and XT registers
; 5) LRETR - this will also clear the RPC
;    register since 0 was on the stack
;-----------------------------------------------

_ExitBoot:

;-----------------------------------------------
;   Insure that the stack is deallocated
;-----------------------------------------------

    MOV SP,#__stack

;-----------------------------------------------
; Clear the bottom of the stack.  This will endup
; in RPC when we are finished
;-----------------------------------------------

    MOV  *SP++,#0
    MOV  *SP++,#0

;-----------------------------------------------
; Load RPC with the entry point as determined
; by the boot mode.  This address will be returned
; in the ACC register.
;-----------------------------------------------

    PUSH ACC
    POP  RPC

;-----------------------------------------------
; Put registers back in their reset state.
;
; Clear all the XARn, ACC, XT, and P and DP
; registers
;
; NOTE: Leave the device in C28x operating mode
;       (OBJMODE = 1, AMODE = 0)
;-----------------------------------------------
    ZAPA
    MOVL  XT,ACC
    MOVZ  AR0,AL
    MOVZ  AR1,AL
    MOVZ  AR2,AL
    MOVZ  AR3,AL
    MOVZ  AR4,AL
    MOVZ  AR5,AL
    MOVZ  AR6,AL
    MOVZ  AR7,AL
    MOVW  DP, #0

    MOV  *SP++,#0
    MOV  *SP++,#0x0A0B
    POP  ST1
    POP  ST0

;------------------------------------------------
;   Jump to the EntryAddr as defined by the
;   boot mode selected and continue execution
;-----------------------------------------------

    LRETR

;eof ----------

  • 并不是把ACC的值放到RPC,而是把原来LCR指令压倒堆栈的RPC值pop回来,具体请看SPRU430F的220页。

    Long call using return PC pointer (RPC). The current RPC value is pushed onto the
    software stack, pointed to by SP register, in two 16-bit operations. Next, the RPC
    register is loaded with the return address. Next, the 22-bit immediate destination address
    is loaded into the PC:
    [SP] = RPC(15:0);
    SP = SP + 1;
    [SP] = RPC(21:16);
    SP = SP + 1;
    RPC = PC + 2;
    PC = 22bit;
    Note: The LCR and LRETR operations, enable 4 cycle call and 4 cycle return. The
    standard LC and LRET operations only enable a 4 cycle call and 8 cycle return. The
    LCR and LRETR operations can be nested and can freely replace the LC and LRET
    operations. This is the case on interrupts also. Only on a task switch operation, does the
    RPC need to be manually saved and restored.

  • 2.2.8 Return Program Counter (RPC)
    When a call operation is performed using the LCR instruction, the return address is saved in the RPC
    register and the old value in the RPC is saved on the stack (in two 16-bit operations). When a return
    operation is performed using the LRETR instruction, the return address is read from the RPC register and
    the value on the stack is written into the RPC register (in two 16-bit operations). Other call instructions do
    not use the RPC register. For more information, see the instructions in Chapter 6.

    读了上面一段还是不解,是不是跟函数嵌套有关, EntryAddr是作为RPC的 old value压入stack,而运行完LCR _main RPC放的是SCI_Boot的地址

    LCR _main

    Uint32 mian()

    {......

     return SCI_Boot();

    }

    Uint32  SCI_Boot()

    {......

     return EntryAddr;

    }