This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D CPU1烧录STANDALONE,离线不运行

先说下我的操作过程,用的开发板是TI的TMDXDOCK28377D:

1、板子SW1都是UP(1)(boot mode),A:SW1(ISO、UART)

2、供电,连接板上的下载USB

3、打开CCS,导入blinky_dc两个工程(V200--dual),开始时候CPU1和CPU2都是RAM-ACTIVE的,两个工程分别

      右键->Properties->General->Configuration->Manage Configurations   ->   CPU1_FLASH_STANDALONE (ACTIVE)   和 CPU2_FLASH(ACTIVE)->OK

4、右键工程-> 分别Build Project    生成.OUT   (有警告,都是说编译器版本问题的,#10190-D,#10272-D)

5、用CPU1的Target Configurations ->launch,CPU1和CPU2都连接,

     点击CPU1->LOAD->CPU1_FLASH_STANDALONE->OK,点击CPU2->LOAD->CPU2_FLASH->OK

6、关电源,拔掉USB下载线,A:SW1(J-TAG,UART)

7、上电,LD2和LD3没反应

8、单独试CPU1也是运行不起来

不知道哪里出错,现在一个头两个大,急死我了,  谢谢大家了!

  • 确保你的CMD是flash的    然后生成.out

    如果你的cmd是flash的   然后你选择debug时   会弹出擦除  烧写的进度条

    然后等烧写完了   在上电会执行的     还有boot模式可以改变一下试试