This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP f28335不同运行频率下核心供电问题与手册提供信息存在差异的问题



本人应用F28335用于某设备的控制,过程中出现一些问题,经查资料怀疑与核心供电有关系,手册上提供的信息是F28335运行在100MHz时核心供电应为1.8v并小于1.89v,150MHz时1.9v并应小于1.99v,而我在实际应用时系统运行在100MHz,核心供电2.15v,虽未出现问题,但感觉已经到达安全边界,损坏的概率增大,经过调整后,核心供电降低至1.89以下,却出现了无法利用仿真器烧写程序的问题,甚至加大至1.95v时仍无法烧写程序,仿真器为XDS100v2。

有以下问题请教,核心供电在不同运行频率下最大的安全极限是多少,有助于我对产品进行安全设计。

程序烧写问题与核心供电的问题,100MHz运行时,核心供电必须大于1.9V多才可正常烧写,为什么。

烦请TI相关技术人员尽快答复,谢谢!