ccs6.0 里编译成功后,debug时好时坏,dsp为28335,仿真器瑞泰创新的xds200u。
配置目标文件里选的是xds 200 usb emulator,TMS320F28335;仿真器驱动应该是装好了,端口里显示xds2xx Emulator CDC Serial Port (COM9) 和xds2xx User CDC Serial Port (10)。
点击debug 后,目标板能连接上,但是无法运行。
test connection为:
An error occurred while soft opening the controller.
-----An error has occurred and this utility has aborted------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06) .
The title is 'SC_ERR_ECOM_EMUNAME' .
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
另外debug 下拉菜单里有工程名和配置文件(.ccxml),应该点击哪个?有什么区别?