TI工程师,你们好!我下面有三个flash的cmd相关问题:
1、flash cmd文件中的CSM_RSVD 部分和CSM_PWL部分是固定在flash区间上的吗?
2、这两部分能不能修改到其它扇区?(TI提供的都是在FLASHA中)
3、修改后有可能会导致哪些问题?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师,你们好!我下面有三个flash的cmd相关问题:
1、flash cmd文件中的CSM_RSVD 部分和CSM_PWL部分是固定在flash区间上的吗?
2、这两部分能不能修改到其它扇区?(TI提供的都是在FLASHA中)
3、修改后有可能会导致哪些问题?
谢谢!
您好!我目前在调试F2810的板子,不小心把密码区改了,原版如下:
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
OTP : origin = 0x3D7800, length = 0x000800 /* on-chip OTP */
FLASHJ : origin = 0x3D8000, length = 0x002000 /* on-chip FLASH */
FLASHI : origin = 0x3DA000, length = 0x002000 /* on-chip FLASH */
FLASHH : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
/* ZONE7 : origin = 0x3FC000, length = 0x003FC0 /* XINTF zone 7 available if MP/MCn=1 */
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM available if MP/MCn=0 */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* The Flash API functions can be grouped together as shown below.
The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd
and _Flash28_API_RunStart are used to copy the API functions out
of flash memory and into SARAM */
Flash28_API:
{
-lFlash2810_API_V210.lib(.econst)
-lFlash2810_API_V210.lib(.text)
} LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_Flash28_API_LoadStart),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart),
PAGE = 0
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
/* User Defined Sections */
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > RAMH0 PAGE = 1
.esysmem : > RAMH0 PAGE = 1
/* Initalized sections go in Flash */
/* Needs to be on page 0 for SDFlash to program it */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHC PAGE = 0 /* Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
改后如下:
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
OTP : origin = 0x3D7800, length = 0x000800 /* on-chip OTP */
FLASHJ : origin = 0x3D8000, length = 0x002000 /* on-chip FLASH */
FLASHI : origin = 0x3DA000, length = 0x002000 /* on-chip FLASH */
FLASHH : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E8000, length = 0x003F80 /* on-chip FLASH */
FLASHD : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3EBF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3EBFF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3EBFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
/* ZONE7 : origin = 0x3FC000, length = 0x003FC0 /* XINTF zone 7 available if MP/MCn=1 */
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM available if MP/MCn=0 */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* The Flash API functions can be grouped together as shown below.
The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd
and _Flash28_API_RunStart are used to copy the API functions out
of flash memory and into SARAM */
Flash28_API:
{
-lFlash2810_API_V210.lib(.econst)
-lFlash2810_API_V210.lib(.text)
} LOAD = FLASHE,
RUN = RAML0,
LOAD_START(_Flash28_API_LoadStart),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart),
PAGE = 0
/* Allocate program areas: */
.cinit : > FLASHE PAGE = 0
.pinit : > FLASHE, PAGE = 0
.text : > FLASHE PAGE = 0
/* User Defined Sections */
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHE,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > RAMH0 PAGE = 1
.esysmem : > RAMH0 PAGE = 1
/* Initalized sections go in Flash */
/* Needs to be on page 0 for SDFlash to program it */
.econst : > FLASHE PAGE = 0
.switch : > FLASHE PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHE PAGE = 0 /* Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
(现在在做bootloader 想把bootloader只放进E扇区,上面的阴影部分是我改动的部分)
之后我刷程序,第一次成功之后,再刷时候一直刷不进去,报如下的错误:
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: GEL: File: C:\Users\Administrator.USER-20161128MX\Desktop\tidcs\c28\DSP281x\
v120\DSP281x_examples_ccsv4\ecan_back2back\Debug\Example_281xECanBack2Back.out: Load failed.
这种情况是不是把芯片锁了?有没有解决的办法呢?
谢谢!
好的,谢谢您的回答!我现在就是烧官网上例程也烧不进去,报的错误就是:
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: GEL: File: C:\Users\Administrator.USER-20161128MX\Desktop\tidcs\c28\DSP281x\
v120\DSP281x_examples_ccsv4\ecan_back2back\Debug\Example_281xECanBack2Back.out: Load failed.
没改cmd文件之前一直没事,这种情况是不是芯片锁住了,有什么解决办法吗?
非常感谢!
那你可以不烧录程序,而仅先连接仿真器吗?
如果可以,请查看一下flash能否被擦除,或者根据.cmd文件查看一下密码区是否有数据,如果看到的全是0,包括整个flash,那么就是被加密了,你可以先解密芯片后再操作。相信你是有密码的,所以可以通过on-chip flash programmer完成。如果不是为0,那说明芯片没有被加密,程序不能被烧录是其它原因。
查看地址0x3F 7FF8到0x3F 7FFF的区间内,是否为全0xFFFF,是就说明没有加密,全0x0000表示加密。
如果没有加密,你可以试试单独擦除是否成功,如果不成功,会报什么错错误,根据提示去分析问题。
您好!顺便问一下如果我把bootloader放入A扇区,应用程序想放入D扇区,请问应用程序的cmd文件应该怎么修改呢?
因为在cmd文件中CSM_RSVD、BEGIN 、CSM_PWL这三个储存空间总是连续的,并且BEGIN总是夹在另外两个中间,cmd还要求空间必须连续,要改BEGIN必须会改另外两个区间,而另外两个的空间又必须在FLASHA中,也就是说BEGIN也必须在FLASHA中,。这样就矛盾了,该怎么改呢?谢谢您!
在另外一个新建的帖子里已由TI的同事回答:
http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56/t/121206.aspx