This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP 28377 程序跑步下去,大牛帮我看看cmd文件和map文件是否有问题



程序RAM中运行,单步调试一直在

PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
PieCtrlRegs.PIEIER1.bit.INTx2 = 1;
PieCtrlRegs.PIEIER1.bit.INTx3 = 1;
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

#ifdef _FLASH
// Send boot command to allow the CPU2 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
// Send boot command to allow the CPU2 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif

跳来跳去,就是不执行我下面的while(1)死循环。

**ps  程序有时能够执行下去,但是执行顺序与理想状态有很大的差距,调用函数时的参数值和实际函数跑起来的同一参数值大小不同。

由于程序量的增大,对官方的CMD的文件进行一定的修改(原来.text 分配的大小不能满足现在的需求)

这是什么原因呢?和CMD有关系吗?

附件中我的CMD文件

  • 如果你是仿真的情况下,需要将下面的语句屏蔽掉。因为这个是引导CPU2 的,和CPU2 ROM中的bootloader代码通信,如果CPU2 没有跑在ROM,则会死机在那里。

    #ifdef _FLASH
    // Send boot command to allow the CPU2 application to begin execution
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
    #else
    // Send boot command to allow the CPU2 application to begin execution
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
    #endif

    ERIC