技术参考手册中介绍采样/保持时间由系统时钟决定,转换时间由ADCCLK时间确定,在数据手册中给出了采样保持时间设定的一些参数;
我的疑问是文档中提到12位AD转换大约需要10.5 ADCCLK周期,16位AD转换大约需要29.5 ADCCLK周期,通过配置ADCCTL2寄存器中的PRESCALE位可以配置ADCCLK频率,但是当我使用16位采样模式时,29.5 ADCCLK周期是通过配置哪个寄存器体现出来的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
技术参考手册中介绍采样/保持时间由系统时钟决定,转换时间由ADCCLK时间确定,在数据手册中给出了采样保持时间设定的一些参数;
我的疑问是文档中提到12位AD转换大约需要10.5 ADCCLK周期,16位AD转换大约需要29.5 ADCCLK周期,通过配置ADCCTL2寄存器中的PRESCALE位可以配置ADCCLK频率,但是当我使用16位采样模式时,29.5 ADCCLK周期是通过配置哪个寄存器体现出来的?
我的疑问是文档中提到12位AD转换大约需要10.5 ADCCLK周期,16位AD转换大约需要29.5 ADCCLK周期,通过配置ADCCTL2寄存器中的PRESCALE位可以配置ADCCLK频率,但是当我使用16位采样模式时,29.5 ADCCLK周期是通过配置哪个寄存器体现出来的?
ERIC: 还是通过ADCCTL2里面的分频设置。这里只是谈到转换要多少个ADC CLK, 至于时钟频率,就看ADC的时钟配置寄存器。
另外要注意的一点是,12位的ADC和16位的ADC 采样保持窗口设置也不一样,后者更长,参考controlSUITE ADC例程。
仔细阅读了这部分文档,基本理解时钟设置的问题了,现在发现使用16位模式采样得到电压换算后为1.496V,实际电压信号为1.499V,这个采样误差可以消除吗?
感谢你的回复,已经找到原因了,TI文档中说明AD采样部分需要在每一个参考电压引脚附近接一个电容,我的硬件设计忽略了这个问题,电压基准后接的电容数量及容值都不够,导致采样结果不正确,增加电容后采样结果正确;还有官方例程中好像都是针对12位AD 的配置,参考意义不大,根据需要AD采样时序设置好采样、保持、转换各个阶段时间即可,很低级的错误...