This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

给28027F添加dlog出现问题

我是做28027F无感控制PMSM,用的是motor ware里面的lab1b程序,想给里面添加一个dlog,但是添加完以后,编译出现如下警告

Description Resource Path Location Type
#10247-D creating output section "DLOG" without a SECTIONS proj_lab01b    C/C++ Problem

然后我在28027.cmd文件里面为dlog创建了一个sections,此时警告消失,编译没有问题,但是下载到板子上以后,程序就直接到一个中断里面死循环,

interrupt void PIE_illegalIsr(void)
{
    // The next two lines are placeholders
    asm(" ESTOP0");
    // endless hold loop
    for(;;);
} // end of PIE_illegalIsr() function
是我sections创建不对吗,应该改成什么样,我对照datasheet上面的。实在找不到地方了,请大神帮帮忙解解惑,万分感谢。
下面是我的.cmd文件,我试着给dlog添加过好多次sections,但都会死在中断里面,dlog的长度是400。
MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
  // L0 SARAM    : origin = 0x3F8000, length = 0x000400
   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA     /* IQ Math Tables in Boot ROM */
   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
//   FLASHB_D    : origin = 0x3F0000, length = 0x005C00
   FLASHB_D    : origin = 0x3F0000, length = 0x006000     /* on-chip FLASH B, C and D */
   D_FLASHA    : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH A */
   P_RAML0     : origin = 0x008000, length = 0x000980     /* on-chip PRAM block L0 */

   //FLASHB_C    : origin = 0x3F5C00, length = 0x000400
   //G_RAML0     : origin = 0x3F8000, length = 0x000400

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   RAMM0_M1    : origin = 0x000000, length = 0x000600     /* on-chip RAM block M0 + M1. 0x600 to 0x800 reserved for InstaSPIN */
     /* on-chip DRAM block L0 */
   D_RAML0     : origin = 0x008980, length = 0x00680    /* on-chip RAM block M1 */
  // G_RAML0     : origin = 0x3F8C00, length = 0x000400
}
/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHB_D     PAGE = 0
   .pinit              : > FLASHB_D,    PAGE = 0
   .text               : > FLASHB_D     PAGE = 0
   codestart           : > BEGIN        PAGE = 0
   ramfuncs            : LOAD = FLASHB_D,
                         RUN = P_RAML0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0
   csmpasswds          : > CSM_PWL_P0   PAGE = 0
   csm_rsvd            : > CSM_RSVD     PAGE = 0
   /* Allocate uninitalized data sections: */
   .stack              : > D_RAML0     PAGE = 1
   .ebss               : > RAMM0_M1     PAGE = 1
 // .ebss               : > RAMM0     PAGE = 1
  .esysmem            : > RAMM0_M1     PAGE = 1
 //  .esysmem            : > RAMM0     PAGE = 1
   ebss_extension      : > P_RAML0      PAGE = 0
  rom_accessed_data   : > RAMM0_M1     PAGE = 1
//   rom_accessed_data   : > RAMM0     PAGE = 1
   vib_buf_data        : > D_RAML0      PAGE = 1
   graph_data     : > D_RAML0      PAGE = 1
   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > D_FLASHA,    PAGE = 0
   .switch             : > D_FLASHA,    PAGE = 0
   /* Allocate IQ math areas: */
   IQmath              : > FLASHB_D     PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,    PAGE = 0, TYPE = NOLOAD
   /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {
              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
   }
   */
   /* Uncomment the section below if calling the IQNasin() or IQasin()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables3
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
   {
              IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
   }
   */
   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.  */
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
}
 SECTIONS
{
 DLOG: > D_RAML0,PAGE=1
 }