This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs5错误提示 DWARF 问题



warning #99922: C:\Users\Jerry\AppData\Local\Temp\039282: failed to locate
>> Compilation failure
   DWARF abbreviation code 92 in the abbreviation table at offset 0x00000000;
   skipping remainder of compile unit at offset 0x0006366a
warning #99922: C:\Users\Jerry\AppData\Local\Temp\039282: failed to locate
   DWARF abbreviation table at offset 0x00000090; skipping remainder of compile
   unit at offset 0x00063a83
DIAG/user_msg_api.c:241:internal fatal error #99926: (dwarf_error_handler():
   C:\Users\Jerry\AppData\Local\Temp\039282: internal error:  NULL die
   references are not allowed)
INTERNAL ERROR: C:\ti\ccsv5\tools\compiler\c2000_6.1.0\bin\lnk2000.exe aborted