This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28377D 程序跑入interrupt void PIE_RESERVED_ISR(void)原因



用DSP28377D写CAN的fifo接收问题,按一下步骤每次都会跑入interrupt void PIE_RESERVED_ISR(void):

1、下载程序----2运行程序-----3.can盒发数据-----4、程序跑入interrupt void PIE_RESERVED_ISR(void)

现在我想看看是什么原因导致程序跑入interrupt void PIE_RESERVED_ISR(void),所以想定位在程序跑入interrupt void PIE_RESERVED_ISR(void)之前是在执行哪段程序,请问怎么做?

另外,如果restart一下程序,则程序就不会再次跑进interrupt void PIE_RESERVED_ISR(void)了,并且接收到的数据正常。

请高手指点怎么定位跑入interrupt void PIE_RESERVED_ISR(void)中断前的执行情况,非常感谢了。