DMA中断的优先级要比AD中断的优先级低,所以两个同时触发DMA也要排在后边,然后将AD转换生成的结果搬移,可以实现吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DMA中断的优先级要比AD中断的优先级低,所以两个同时触发DMA也要排在后边,然后将AD转换生成的结果搬移,可以实现吗
您好,Emma Wang1!
您说的是ePWM的SOC触发AD中断转换数据,然后AD的SEQ1触发DMA搬移吗?如果是都通过SOC触发的话,有可能实现吗,我并没有找到相关的例程,而且在DMA定义中,触发源的定义虽然备注里写了,但是定义的时候并未涉及ePWM的SOC触发DMA,这是为什么呢?可能有些是我理解错误,提的问题比较可笑,请见谅,谢谢!
对于你第一个问题,理论上是可以的,实际上DMA的读取结果可能不是ADC的转换结果,所以一般不会这么用。
DMA触发源的定义在DMA.h中:
struct MODE_BITS { // bits description
Uint16 PERINTSEL:5; // 4:0 Peripheral Interrupt and Sync Select Bits (R/W):
// 0 no interrupt
// 1 SEQ1INT & ADCSYNC
// 2 SEQ2INT
// 3 XINT1
// 4 XINT2
// 5 XINT3
// 6 XINT4
// 7 XINT5
// 8 XINT6
// 9 XINT7
// 10 XINT13
// 11 TINT0
// 12 TINT1
// 13 TINT2
// 14 MXEVTA & MXSYNCA
// 15 MREVTA & MRSYNCA
// 16 MXEVTB & MXSYNCB
// 17 MREVTB & MRSYNCB
// 18 ePWM1SOCA
// 19 ePWM1SOCB
// 20 ePWM2SOCA
// 21 ePWM2SOCB
// 22 ePWM3SOCA
// 23 ePWM3SOCB
// 24 ePWM4SOCA
// 25 ePWM4SOCB
// 26 ePWM5SOCA
// 27 ePWM5SOCB
// 28 ePWM6SOCA
// 29 ePWM6SOCB
// 30:31 no interrupt