各位老师好,最近开始学习使用28335DSP,但是使用100v2仿真器出现问题,当debug as以后会报
XDS2XX USB DEBUG PROBE 0/C28XX:Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 7.0.48.0)
但是我使用的是100v2仿真器啊,100v3也试用过也是报这个故障。
需要提起的是,开始以为是系统和软件版本的问题,同时使用同事的IBM笔记本可以正常连接,所以装了和同事一样的win10专业版。同时ccs软件也从原来的6.1更新为7.3.,但是全部重装依然报这个错。
请问这个问题是什么原因,该如何解决,感谢各位不吝赐教。