我用的开发板是Digitally Controlled Solar Micro Inverter Design using C2000 Piccolo Microcontroller 。
在进行DCDC部分MPPT闭环实验时,变压器会发出响声而且持续一会后电路断开,EPWM3故障标志显示过流保护,但我设置的光伏开路电压38V,短路电流1.5A,实际电流最高也就限制在1.5A 。 为什么会发生过流保护呢?我看程序中电流限制是10A 。还有SolarMicroInv-Main.c中的保护程序里COMP3的输入电压a在哪里配置呢?我在SolarMicroInv-DevInit_F2803x.c、SolarMicroInv-Settings.h、SolarMicroInv-Includes.h中都没有找到。
谢谢大家!
保护代码如下:
//TODO Protection Code
EALLOW;
EPwm1Regs.TZSEL.bit.CBC6 = 0x1;
EPwm2Regs.TZSEL.bit.CBC6 = 0x1;
EPwm3Regs.TZSEL.bit.CBC6 = 0x1;
EPwm1Regs.TZSEL.bit.OSHT2 = 0x1;
EPwm2Regs.TZSEL.bit.OSHT2 = 0x1;
Comp3Regs.COMPCTL.bit.SYNCSEL =0x0; // asynchronous version of the COMP signal is passed to the EPWM/GPIO module
Comp3Regs.COMPCTL.bit.CMPINV =0x0; // Output of the comparator is passed directly
Comp3Regs.COMPCTL.bit.COMPSOURCE =0x0; // inverting input of the comparator is connected to the internal DAC
Comp3Regs.DACVAL.bit.DACVAL =700; // set DAC input to peak trip point ~10 Amps, full scale is 15Amps
AdcRegs.COMPHYSTCTL.bit.COMP1_HYST_DISABLE = 0x1;
EPwm3Regs.DCTRIPSEL.bit.DCAHCOMPSEL=DC_COMP3OUT ;
EPwm3Regs.TZDCSEL.bit.DCAEVT1=TZ_DCAH_HI;
EPwm3Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT_FLT ;
EPwm3Regs.DCACTL.bit.EVT1FRCSYNCSEL=DC_EVT_ASYNC;
EPwm3Regs.TZSEL.bit.DCAEVT1=0x1;
EPwm3Regs.DCFCTL.bit.BLANKINV=DC_BLANK_NOTINV; // Blanking window is not inverted
EPwm3Regs.DCFCTL.bit.SRCSEL=DC_SRC_DCAEVT1; //DCAEVT1
EPwm3Regs.DCFCTL.bit.PULSESEL=DC_PULSESEL_PRD; // apply offset from TBCTR=TBPRD
EPwm3Regs.DCFOFFSET=59;
EPwm3Regs.DCFWINDOW=255;
// TZA events can force EPWMxA
// TZB events can force EPWMxB
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EPwm3Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB will go low
EPwm1Regs.TZCLR.bit.OST = 1;
EPwm2Regs.TZCLR.bit.OST = 1;
EPwm3Regs.TZCLR.bit.OST = 1;
EPwm1Regs.TZFRC.bit.OST = 0x1;
EPwm2Regs.TZFRC.bit.OST = 0x1;
EPwm3Regs.TZFRC.bit.OST = 0x1;
EDIS;