采用16位ADC,一个用A2,A3,另一个用A4,A5,当调节A2,A3的电压值时,A4,A5软件采集的电压值也会发生变化,为什么?有没人人知道原因?/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用16位ADC,一个用A2,A3,另一个用A4,A5,当调节A2,A3的电压值时,A4,A5软件采集的电压值也会发生变化,为什么?有没人人知道原因?/
“
(Vp + Vn)/2 任何时刻都必须保证在 Vref/2 正负50mv以内。这句话不是很理解,是不是说放大器的 地,与28377的基准地两个地是虚地,不接到一起?不然无法保证Vp + Vn)/2 任何时刻都必须保证在 Vref/2 正负50mv以内.
”
就是你Vp +Vn 任何时刻的共模信号要在 Vref/2 正负50mv以内。
举个例程,如果你的Vref是3V, 你要输入一个1V的信号,
那么Vp=2V, Vn = 1V, (Vp+ Vn) /2 = 1.65V, 这个偏差保证在50mv以内。
有些外置的差分ADC芯片能够接受伪差分信号,如Vn 接地, Vp输入单端信号如0~3V, 那么这个时候(Vp + Vn)/2 就是在0~1.65V波动的。
F2837X不能接受这个伪差分输入的形式。你就看你实际的输入信号,是否能在任何时刻都能保证这个条件。
至于参考电路,你参考THS4521的手册即可。